Yujie,
I do not have an exact answer for the time, but it should generally be less than two seconds. The patterns can have different level of compression in the Flash memory, so that the time will depend on the decompression into the controller's DDR memory…
Part Number: DLPLIGHTCRAFTER Hi,
Could anyone help me with 3D CAD files for DLP lightcrafter 6500?
Either .stp file or .iges file would be helpful. I found the cad files for DLP2000 but it is not as similar in design as 6500.
Thanks for your time.
…
Part Number: DLPLIGHTCRAFTER Hello,
We purchased your DLP LightCrafter last year, and have been using this website ( www.ti.com/.../dlplightcrafter) to download the DLP LightCrafter Firmware and Software Bundle Version 3.0.
But we just found out after…
Part Number: DLPLCR4500EVM Hello,
I have recently problem start with Lightcrafter GUI.
I am using since long time windows 10 but it was connected with GUI, but last few days I am having a problem with connectivity. DLP detects in my windows 10 system…
Part Number: DLPLIGHTCRAFTER Hi everyone
I am working on the dlpLightcrafter.I want to use stored pattern sequence but it fails.it doesn't upload the sequence images.It says upload failed.here are my two images which i want to use.Here are the details…
Part Number: DLPLIGHTCRAFTER Hello,
As of today,Do you have any plans for the end of production of the DLPLIGHTCRAFTER Evaluation Module?
www.ti.com/.../DLPLIGHTCRAFTER
Best regards, Seishin
Part Number: DLPLIGHTCRAFTER Hello,
I want to buy the DLPLIGHTCRAFTER 4500. But in the datasheet, it is mentioned that it is composed of the DLP4500FQE.
For my application, I need to use the DLP4500FQD.
Is it possible to change the two DLPs ? Does the…
Part Number: DLP3000-C300REF I am using what I think is quite an old version of the DLP Lightcrafter (the manual is DLPU006e - dated 2014), I am having trouble operating the DLP with the GUI DLPLightcrafter V7 - status shows not connected.
I am using…
Part Number: DLPLIGHTCRAFTER Hi:
We got an DLPLIGHTCRAFTER evaluation module around 8 years ago
( www.ti.com/.../DLPLIGHTCRAFTER )
We discovered that the LED luminosity output has decayed to a point that
we have to replace the LEDs for our use.
May I ask…
Part Number: DLPLIGHTCRAFTER Hello,
I intend to purchase a DLPLightCrafter 4500 for my integrated Fringe projection application. Is it possible to load the patterns and program a sequence such that, later it can function directly when the power suppply…