Hi Roland,
Thanks for the additional information. Roughly what percentage of your PCBs are showing this issue?
To clarify my power supply comment, I was referring to the bench top supply or wall wart that you are using as the main system supply. With…
Hi,
That was my initial thought but i wanted to confirm from your side.
OK.
Here is the utility with readme you can download from http://www.ti.com/tool/dlpr300 look for DLPR300SPLASH:
Splash Screen Utility for DLPR300 section. You can download from here…
Hi Kristof,
It was nice talking to you at MN Tech Day.
Like Sanjeev said, looks like the DLPC300 firmware is corrupted so try downloading it from here:
http://www.ti.com/tool/dlpr300
It is available as DLPR300PROM.
Regards
Manasi
Chrstine,
The version is you are referring to is called as PACKAGE VERSION.
This contains firmware for all the components - DM365, MSP430, FPGA and DLPC300 . So download the 3.0 Package, and update every component listed in the package. The other piece…
Hi Seishin,
Thanks for posting these details. Could you provide some additional background:
Could you describe (or provide an picture) of the red color image? Is it a solid red projection?
When the red color image is displayed, does the LightCrafter…
Other Parts Discussed in Thread: DLPC300 , DLPR300 TI,
I am looking at using the DLPC300 controller for a system, I have experience driving the DDC3000 chipset and bit-plane driving for DMDs and have a question about Pattern Input mode.
How is this…
Hello Marco,
Welcome to TI DLP E2E community!
I can definitely help you troubleshoot this since I know exactly what might be causing this.
If you are at the latest DM365 firmware version 5.0 and you can connect to the GUI and see the LED D1 on the top…
Hello Heather,
Yes the fact that you can change the LED current value to something, Set it and retrieve the changed value when you do a Get tells me that the I2C interface between DM365 to FPGA to DLPC300 is correct and working.
There is one piece of…
Hi Ben,
Welcome to DLP & MEMS Section of TI E2E Community!
Download the " DLPR300PROM: Configuration Firmware for DLPC300" from here, http://www.ti.com/tool/dlpr300
This file is named DLPC300_FIRMWARE_OLD.bin in the readme.
Regards,
Divy…