Part Number: DM385 Hi expers,
We have been using DM385 product.
I tried using the TI cross-reference but couldn't find of replacement of DM385 product.
(link: https://www.ti.com/cross-reference-search/singlepart?searchTerm=DM385 )
Could you please…
Part Number: DM385 Hi
I am wondering if this part is provided with an on-chipf the termination resistor for MIPI CSI2 receiver interface? As far I could check, it is neccesary to add a 100ohm termination resistor between P&N.
Can anyone confirm this…
Part Number: DM385 Other Parts Discussed in Thread: DM383 , DM3730 , DM388 , DM505 , DM3725 , DM8107
Hi TI
There's a request that Customer need for DM385 platform' NAND Programming in Factory.
Could you please provide the BCH8 ECC source code which…
Part Number: DM385 Hello,
We are working with a custom board (nSketch) based on the IPNC 3.5 and would like to know how to determine the units for the gains and exposure settings. We would like to understand the autoexposure and digital and analog gain…
Hi,
cbraeuer said: I have tried to implement EncodingPreset=HIGH_SPEED, but as in the manual described, this changes the NALUpreset from USER_DEFINED to DEFAULT, so that the SPS/PPS Headers are gone.
Yes, user can play with NAUL presets when EncodingPreset…
Part Number: DM385 Dear all,
We use the DM385 (DaVinici) for streaming purposes for a surveillance cam (YCbCr (via VIN(0)A_xxx) -> H.264 (via MII Interface). Unfortunately, we have a lot of complains regarding image integrity (overlapping images, distortions…
Part Number: DM385 Tool/software: TI C/C++ Compiler
software version: Ipnc Rdk 3.9.1
I need to slice the data on the VPSs side, such as dividing the 1920 x 1080 frame into four parts, and then passing it to the video side for encoding.
What do I need…
Part Number: DM385 Does BU know if MT29F2G08ABAG can be use as boot NAD of DM385?
Customer use MT29F2G08ABAE before, works right. now micro process upgrade, new MT29F2G08ABAG can't boot. all operation procedure are same. it can be wrote from UART booted…
Part Number: DM385 Hello ,
I am implementing Onvif Profile G.
I have installed ONVIF Device Test Tool ver - 19.12.
I am testing the capabilities APIs for Device. However for now I am testing only __tds__GetServices function in that particularly i am checking…