Part Number: DM505 Hi Team,
Can you confirm the DM505 and TDA3 are both in active production? Are either of these approaching EOL? There is some confusion on our end as to whether or not the TDA3 will be the successor to the DM505.
https://www.ti.com…
Part Number: DM505
Hi Team, Our customer wants to estimate the power consumption of DM505 early on before prototyping. From the datasheet it's case-specific and depends on specific tasks, but they would like to see if we have a ballpark estimate. If they…
Part Number: DM505 I am attempting to configure the EDMA to connect to McSPI2 which is in a slave configuration - if this is important or not. The issue is that I am attempting to incorporate this into the Vision SDK provided SBL that will be loaded into…
Part Number: DM505 Using Code Composer Studio and an XDS200 I am not seeing activity on the DM505 JTAG bus. Thus, I am not able to connect to the Cortex_M4_IPU1_C0 core I am attempting to connect to:
The TCLK signal is functional, but the TDI and TDO…
Part Number: DM505 I am attempting to store some constants at some known address in QSPI memory. I have the Vision SDK installed an I am using the SBL that comes with it. What I want to add to that SBL is to inspect a constant in the QSPI flash that I…
Part Number: DM505 I am trying to use the Blackhawk XDS560v2 with Code Composer Studio v10.3.1.00003, but cannot get the emulator to connect. Oddly, Windows 10 64-bit, cannot locate the device driver - even after pointing to the file location C:\ti\ccs1031…
Part Number: DM505 I am having difficulty locating the IBIS models for the DM505. Do IBIS models exist for this device? If so, where can I find them.
-Andrew