Hi,
Caishuang Yang said: rxGoodFrames = 5 rxBcastFrames = 5 aleDrop = 5
It seems like what ever the packets packets received by Host Port from A72 are droppped due to ALE no match? Can you please dump the packets at A72 using tcpdump --XX option to view…
You may need to purchase the EVM on ti.com: TUSB1046EVM Evaluation board | TI.com
I would recommend you reach out and contact your TI rep to see if anything outside of that can be done.
Regards,
Nicholaus
Other Parts Discussed in Thread: 10G-EXPANSION-EVM Hi
I have the Part number but it is not recognise... Part Number is 10G-EXPANSION-EVM
Please can you provide the CE/EU Declaration of Conformity for 10G-EXPANSION-EVM ?
We, Mouser USA, have this product…
Part Number: TPS65987EVM Hello,
I have to design an interface between a PC that supports Thunderbolt and a system. One video signal and one audio signal are sent to the system from the PC, and there is a USB2 communication between both too (please see…
Part Number: DPS-DONGLE-EVM Other Parts Discussed in Thread: USB2ANY , SIGCONARCHITECT We would like to use the SigCon Architect software to test settings on our existing boards. Depending on the model, our boards have up to 5 TI chips daisy-chained together…
Part Number: TPS65981 Hi,
I want to configure the EVM as a 2 lane DisplayPort + 2 lane USB 3.1 configuration. Are there any steps to do so using the EVM Application Customization Tool?
Thanks.
Part Number: TPS65987D Other Parts Discussed in Thread: 10G-EXPANSION-EVM , TUSB564 Hi Team,
I'm using the TPS65987EVM + 10G-EXPANSION-EVM (sink module). The DP output is working, but the USB3 over the Type-A connector doesn't work.
I checked it…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: TDA4VM Is it possible to obtain the schematic for the QSGMII Ethernet (QPEnet) expansion board that comes with the TDA4VM EVM?
Thanks!
Part Number: DPS-DONGLE-EVM Other Parts Discussed in Thread: MSP430F5529 Hello,
I need a Letter of Volatility for DPS-DONGLE-EVM. I can provide a questionnaire template if a letter is not already available.
Thank you,
Natalie