Part Number: MCU-PLUS-SDK-AM243X Other Parts Discussed in Thread: DP83630 Hi all,
DP83630 datasheet says in section 6.6 that there is a Software Development Guide for the DP83630.
May I know which document it's referring to? I cannot find a exact match…
Hi Srikanth,
srikanth said: can you share example code for udp or tcp/ip protocol for LAUNCHXL2-570LC4357.
(+) [FAQ] TMS570LC4357: Examples and Demos available for Hercules Controllers (E.g. TMS570x, RM57x and RM46x etc) - Arm-based microcontrollers forum…
Part Number: DP83630 Hi,
We are doing the pressure test of DP83630’s PTP and see an issue.
DP83630 works as slave, it receives the sync message and record the T2.
By set PTP_CTL bit4 ( load m clock ), and read PTP_TDR, we can get the time.
Got a wrong…
Part Number: DP83630 Hi All,
I have a question about the DP83630. If I don't use the LED_ACT pin, can I leave it open? Or do you need to do pullups and pulldowns? If the default option is required, then there is no need for external pull-up or pull down…
Part Number: DP83630 Other Parts Discussed in Thread: DP83869 Hi,
We are trying to use DP83630 PHY to design copper SFP, as per block diagram shown below
on DP83630 for above circuit is how to interface clock signals (especially TXCLK and TXEN signals…
Part Number: DP83640 Other Parts Discussed in Thread: DP83630 Team,
From you experience is it possible to design a PCB for both package? (in order to solder the one IC you can source at this point of time) DP83640: 48-pin LQFP Package (7 mm × 7 mm)…
Part Number: DP83630
Dear experts,
Our partner was trying to pre-approve the DP83630SQ ahead of a competitor brand's product.
They brought in parts from TI/Arrow Electronics. Parts were sealed in Original Factory conditions. During IQC, random pieces…
Part Number: DP83630 Hi all,
We have a product where the product owner decided to include two Ethernet PHYs (DP83630 that supports IEEE-1588 PTPv2) for future use such as synchronizing multiple boards and data transfers. The board does not contain an…
Part Number: DP83620 Other Parts Discussed in Thread: DP83630 , Hi Team,
The customer wants to change the DP83630DP83630 with DP83620 and they have some concerns about the Pins23 and 24. They have in their design two DP83630 which are connected like this…
Hello Archie,
Thank you for the mail and the inputs.
If you do not have additional question, please click the resolved button to close.
Regards,
Sreenivasa