Part Number: DP83825EVM Other Parts Discussed in Thread: DP83825 hi, team
Is the schematic (snlr041a) of DP83825EVM consistent with the actual DP83825EVM evaluation board?
From the schematic, it shows only two pins of MSP430(pin 46 and pin 47) are connected…
Part Number: DP83825EVM Hi Team,
customer test EVM and found the LED0 is off while powered on.
When connecting EVM with the laptop and running GUI to detect the ID, there is an error message popup.
Please help.
Thanks.
Hi DD,
I regret to inform that the setup with the 2 EVMs did not work. Register access was not cooperating, nor was sustaining link. Again, I want to reiterate that the DP83825EVM is not suitable for a RMII Slave to RMII Slave application.
Aside from…
Part Number: DP83825EVM Other Parts Discussed in Thread: DP83825I , DP83825 In the DP83825I reference schematic, theire are three 33Ohm resistor: RX_D0 conncet to TX_D0 with 33ohm,etc,What's the 33OHM resisror used for? What if I don't use them,what will…
Part Number: DP83825EVM Other Parts Discussed in Thread: DP83825 , TMS320F28388D Hi, when can I expect the release update of the User's Guide. The one on the web is fitting to the old release.
Regards, Holger
Part Number: DP83825EVM Hello
Please can you provide the CE/EU Declaration of Conformity for DP83825EVM ? This does not seem to be available on the T.I website.
Thank you
Chris
Part Number: DP83825EVM Dear Team,
is there an updated version of the snlu239 u ser-guide. It does not seem to cover current hardware revision HSDC045B? I have a board that does not contain jumpers J16, J17, J18, J14, etc.
Regards
Andreas
Part Number: DP83825EVM Hello,
I wanted to test the DP83825EVM from TI.
I have followed all steps described in the user manual, installed the USB2MDIO software and the corresponding MSP430 driver (in different paths but it should not matter?).
However…
OK, I was finally able to get access to a Win 10 PC. That resolved the problem. Funny thing is that I didn't see it written anywhere what the driver compatibility is.
thanks.
Gerome,
I tried looking at what you suggested above but was not successful mostly because the whole exercise was getting a bit unwieldy and I was having a hard time following the instructions for the EEE query (with the whole extended register access…