Hello Evan-san,
I will request the customer if the layout can be shared.
Also, Could you please check the following question about 0x00A0[4:0]?
[1] Register 0x00A0[4:0] has 5 bits, is '01000' = 0% correct? I received the following answer previously, so…
Part Number: DP83867CR Hello,
I am designing a new carrier board for the Conga-SA7 this has a DP83867 on it and uses the SMARC interface to connect to the carrier board. On the carrier board we want to use an Ethernet switch ic with external PHYs to allow…
Part Number: DP83867CR Hello team,
I have several questions.
1. Which pin is related to GPIO LED_3? I could only find LED_0, LED_1 and LED_2.
2. Datahseet says that RXD7 can be configured as LED pin. Is this correct? It seems like RXD7 should be…
Part Number: DP83867CR Hello team,
I am confused because this device has 3 VDDIO options of 3.3V, 2.5V and 1.8V. Is there any functional difference between them? How should I choose which voltage level to use for VDDIO?
Best Regards, Kei Kuwahara
Hi Kailyn,
I don't believe I've asked this before, but are you able to read/write registers? I would also like to check the MAC's voltage level. Is it also operating at 1.8 V, like our PHY is?
Regards,
Alvaro
Part Number: DP83867CR Hello TI team, We are using DP83867CR, for Compliance testing we are referring this document : https://www.ti.com/lit/an/snla239c/snla239c.pdf?ts=1707443888787
We are able to set 10baseT, and 100baseT, for compliance testing. Whenever…