Part Number: DP83867ERGZ-S-EVM Other Parts Discussed in Thread: DP83867IS I am looking to purchase this part but I need to know if it will fit in my enclosure. I cannot fin any information online on the mounting hole pattern. It would be best to have a…
Part Number: DP83867ERGZ-R-EVM Other Parts Discussed in Thread: MSP430F5529 Dear Team,
1. We would like to use the TDR function of DP83867. Can we use EVB to test TDR function?
Many Thanks.
Jimmy
Part Number: DP83867ERGZ-R-EVM Hello team,
On the user guide, it says GPIO_0 is connected to RJ45 Left (Green).
But on the schematics, GPIO_0 is not connected to LED, and GPIO is not meant for driving LED.
Is GPIO_0 statement should be LED_0? Could…
Part Number: DP83867ERGZ-R-EVM Hello,
I need a letter of volatility for the above part number, if available.
I believe this part does not contain any kind of memory, and as such, would not have a LOV - any confirmation would be appreciated.
Thank you…
Hi Frankie,
Thank you for providing the information so clearly. The Center taps bussed together never works, even without the POE circuitry.
We have a POE reference design board here: https://www.ti.com/tool/TIDA-010083
The schematics and BOM are available…
Hi Rahul,
Franz Forstmayr1 said: The two boards can establish a connection but when running an iperf3 measurement or a netAlly LANBERT measurement I can see packet errors of about 0.01%.
I can establish a connection but see udp packet loss with iperf3…
Part Number: TMS320C6678 Hi,
As per the snippet of code, we got the frequency but have some doubts about it.
1. Can we implement it into the all-core or individual core?
2. We used the code (as per the code's snippet) here is the image,
3. After the…
Part Number: DP83867ERGZ-S-EVM Other Parts Discussed in Thread: DP83869HM , DP83869EVM Dear support team,
I'm trying 1000Base-T Compiliance test with capacitive coupling instead of using magnetics.
I understand DP83867ERGZ-S-EVM supports c apacitive coupling…