Part Number: DP83TC811R-Q1 Other Parts Discussed in Thread: DP83TC811 Hello,
we are working with DP83TC811R-Q1 device. We are trying to configure start-up sequence to get Ethernet communication between devices. I found discrepance information in following…
Part Number: DP83TC811R-Q1 Other Parts Discussed in Thread: DP83TC811 Hi Team,
PHY_AD[3:0] configured by Boot strap cannot be accessed correctly. Is there any possible reason?
<Details> RX_ER(pin-14) and RX_DV(pin-15) are opened. According to Table…
Part Number: DP83TC811R-Q1 Hi,
Do we need to use any specific connector for the communication of 100Base-T1? If so why is it mandatory to use a connector compatible for 100Base-T1.
Is there any suggestion for automotive sealed connector apart from TE…
Part Number: DP83TC811R-Q1 Other Parts Discussed in Thread: DP83TC811 Hello,
we are working with DP83TC811R-Q1 connected with LAN7801 device. I would like to configure DP83TC811R-Q1 register in order to have ethernet interface available after POR.
I checked…
Part Number: DP83TC811R-Q1 Other Parts Discussed in Thread: DP83TC811 Hi TI Experts,
Our DP83TC811R-Q1 has an unlink problem. And when we check the LSR Register 0x0133, the BIT_12 LinkStatus = 1, but BIT_0,1,2 are zeros.
What problems dose this Register value…
Part Number: DP83TC811R-Q1 Other Parts Discussed in Thread: DP83TC811 Hello Expert,
The customer did high temperature testing for DP83TC811R-Q1 and there was a link-down issue happen. After checking the register value, only 0x0017 becomes different. When…
Part Number: DP83TC811R-Q1 PHY receive data issue
after systems start up, can not see any data received from DP83TC811R-Q1 transceiver
PHY is link up, SQI = 75,
during running time, we log the some registers value for your reference (all is hex value) …
Part Number: DP83TC811R-Q1 We currently use DP83TC811RWRNDTQ1 chip as the PHY chip of the BroadR-Reach interface of our imaging radar, and the test found that the output data of the BroadR-Reach interface stops abnormally under the condition of long-term…
Part Number: DP83TC811R-Q1 Other Parts Discussed in Thread: DP83TC811 Hi Team,
How to configure the 100Base-TX Full-Duplex?
I find the 0x0001 is a read-only register.
Thanks,
Xiaoxiang
Part Number: DP83TC811R-Q1 Other Parts Discussed in Thread: TDA2 , DP83TC811 Hi team,
One of our customer's issues, I'm forwarding it below, could you please provide some troubleshooting suggestions
SOC: TDA2
LINUX: 4.19.73
It uses the DP83TC811 driver…