Part Number: DP83TC811-Q1 Other Parts Discussed in Thread: DP83TC811EVM This request is not focused on TC811 only but more a general question
Are there differences in drive strengths between the different T1 PHYs we offer?
Or is there possiblity to amplify…
Part Number: DP83TC811S-Q1 Hi,
In the previous post there is a solution suggested for a unidirectional to bidirectional converter solution. From 100BASE-T1 to Ethernet 100Base-TX, using DP83822 as an intermediate.
Could you give support on how the connection…
Part Number: DP83TC811S-Q1 Other Parts Discussed in Thread: DP83TC811 , DP83TC811EVM Hello!
We are using a normal RJ-45 connector and therefore we have TX+/TX- and RX+/RX- pairs.
Your IC has bidirectional pins so we dont understand how TX and RX should…
Part Number: DP83TC811S-Q1 Hi,
I have some questions about Auto-Polarity Detection and Correction.
1. First question is about device compatiblity. Here is my thought. When DP83TC811S-Q1 is slave, it can detect the polarity and correct automatically no matter…
Part Number: DP83TC811S-Q1 HI Team,
Please let me know if TI has PHY which support TX interface and It is AEC qualified. Our host interface is SGMII and RGMII. Also connect me through mail to elaborate my requirement.
Regards
Manoj A
lu mingdong said: Do I need to configure according to Table 3-2?
Yes, correct.
LED_0 strap will configure the PHY in master/slave mode but the OA configuration as described in the appnote has to be configured for the functional operation of the PHY.
Regards…
Part Number: DP83TC811S-Q1
Hi, TI team
From register PLR_CFG1, bits 12 to 13, can I see the polarity of the current ethernet connection?
According to our test, after normal connection and reverse connection of pins 12 and 13, the values of these two…
Part Number: DP83TC811S-Q1 Other Parts Discussed in Thread: DP83TC811 step:
1. 0x0475 has been set to 0x2000 or 0x3000;
2. and there is no power down or reset;
3.swap the two wires of the MDI and reconnect;
4.wait a few seconds;
5.read register 1, return…
Part Number: DP83TC811S-Q1 Dear TI friends
Does DP83TC811S-Q1 pass the certification of FTZ/UHN/C&S?
How to get the FTZ/UHN/C&S reports for DP83TC811S-Q1?
Thanks.
Part Number: DP83TC811S-Q1 Hi Expert:
Our Customer designing Ethernet PHY into Gateway they are request DP83TC811S-Q1 Functional Safety FIT Rate, FMD and Pin FMA report, could you please help support the requirement?
thank you
Roy