Part Number: DRA71XEVM
Tool/software: Code Composer Studio
Hi,
I have installed Processor Linux SDK v6 and I am working with DRA71x family.
Could you please recommend the best approach to start developing firmware for IPU (Cortex-M4) when it comes to…
Part Number: DRA71XEVM Tool/software: TI C/C++ Compiler Hello, I use 06.00.00.03 version SDK on 16.04 LTS of ubuntu. When i executed ./setup.sh the "yocto-layers" and "config" folder were created outside of ti-processor-sdk-linux-automotive_dra7xx-evm_06_00_00_03…
Part Number: DRA71XEVM
Hello,
I am trying to setup build environment by following the below guide
I have followed all the steps as per that guide.
At the end when i executed build-core-sdk dra7xx-evm, i am getting below error:
user@Temp:~/Prasad/ti…
Part Number: DRA71XEVM Other Parts Discussed in Thread: SYSBIOS , DRA71
Tool/software: TI C/C++ Compiler
Hello,
I need to prepare firmware for IPU1 (EVMDRA71x) with DCAN driver and IPC communication. I do not have JTAG and I'm building everything from the…
Part Number: DRA71XEVM According to the power management section of the Linux SDK processor, there must be a set of virtual files in the /sys/devices/system/cpu/cpu0/cpufreq/:
/sys/devices/system/cpu/cpu0/cpufreq/scaling_available_governors /sys/devices…
Part Number: DRA71XEVM HI.
1. Used usbboot-stand-alone, dfu-util can boot j6entry in Ubuntu linux
2. However, due to the project requirement, we need the host tool like usbboot-stand-alone in Windows. Is there such a host tool in windows?
Thanks.
Part Number: DRA71XEVM Other Parts Discussed in Thread: DLP3030-Q1 , DRV8889-Q1 , Hello Guys,
Good day!
Our customer is
Customer looking to incorporate the following devices for their Heads Up Display Application: DLP3030-Q1 Electronics Evaluation Module;…
Part Number: DRA71XEVM Other Parts Discussed in Thread: DRA71 Hello Guys,
Good day.
Does the DRA71XEVM have any libraries for accessing the RGB data from the camera module over CSI interface?
Thanks to confirm!
Art
Part Number: DRA71XEVM Other Parts Discussed in Thread: DRA718 hi all experts,
my board is custom board with soc DRA711, and DDR3 is 512M, now i run visionSDK in IPU2, but VPS init fail, log as following:
2.685902 s: SYSTEM: VPDMA Descriptor Memory Address…