Part Number: DRA829VXEVM Our PCIe Backplane looks like it is workoing.
But we have one question, does Host side chip must support NTB for Backplane ?
for example:
DRA829VXEVM setted to EP with Backplane.
we have two RC connect to DRA829VXEVM , so does my…
Part Number: DRA829VXEVM We want to evaluate dra829 / tda4xm two processors. We want to buy EVM board. The User's Guide on the official website shows that j721e / dra829 / tda4xm is the same EVM. Can I test dra829 / tda4xm two processors by buying dra829vxevm…
Part Number: DRA829VXEVM We try to enable „PCIe Backplane“ in TI chip.
So follow the “processor-sdk-linux-docs” add "k3 - j721e - pcie - backplane.dtso"
But we get error below(dmesg):
0.568502] pci_epf_ntb pci-epf-ntb: Failed…
Part Number: DRA829VXEVM Hello experts,
Is it possible to change affinity of eth0 interrupts on DRA829 evm working on Linux (ti-processor-sdk-linux-automotive-j7-evm-07_00_01, kernel: Linux j7-evm 5.4.40-g66cf445b76)?
Call to irq_set_affinity returns error…
Part Number: DRA829VXEVM Hi!
I am using Jacinto7 J721E/DRA829/TDA4VM Evaluation Module.
In my kernel module I'd like to add toggling of a few GPIO pins in order to see timing of those signals on oscilloscope.
Which header and/or test points and which…
Part Number: DRA829VXEVM Hi, TI members.
I’m tried to run a single camera demo application by shell command ‘run_app_single_cam.sh’.
I have an EVM board connected Fusion Board (revB) and D3-IMX390-CM camera module.
And I’m using the…
Part Number: DRA829VXEVM Hi everybdoy ,
I m on DRA829 evm , working on Linux .
now I would like to access some GPIO with a scope , moving these pins during code so to run measures on timing , jtters etc
do you have any example on how to move a GPIOs on…
Part Number: DRA829VXEVM Hi, TI support team.
I'm trying to set HDMI port to display Weston client examples according to the guide .
When I tired 'weston --tty=1 --connector=48 --backend=drm-backend.so' command, error messages shows up as below.…
Part Number: DRA829VXEVM Hi,
I'm running the out-of-box single camera demo. I can see the video output on the DP display.
I would like to route the video output to the DSI connector at the bottom of the EVM.
Will it suffice to modify the /vision_apps…