Part Number: DRV-ACC16-EVM I have two DRV-ACC16-EVMs, which show almost the same amplitide and frequency as the other one when measuring acceleration of the same ERM vibration motors by varying RPM with an oscilloscope. This means the acceleration results…
Hey Karan,
Please provide a waveform of Vdrain, VCP, GHA to GND and SHA to GND with gnds of gates and source leveled for clarity.
Not sure about the CP cap damage yet but t is a possibility.
Also please note that the default IDRIVE is the maximum idrive…
Part Number: DRV8353RS-EVM
Hi Friends,
1. INHx and INLx = 0 (Low) GHx Output is =15 V GLx Output is =0 V
2. INHx = 0 (Low) and INLx = PWM GHx Output is =15 V GLx Output is = PWM Output is Correct
3. INHx = PWM and INLx = PWM GHx Output is =26V GLx Output…
Part Number: DRV-ACC16-EVM
Hi Experts,
Good day! Is it possible for you to provide us the x and y distance as on picture pelase? Is it also possible to share the drawing of the product with tolerance?
Thank you in advance.
Best regards,
Jonathan
Part Number: DRV-ACC16-EVM
Hi team,
Here're few questions from the customer may need your help:
1) What is the allowable error for this sensor calibration?
2) Why does the amplitude of the test values of the haptic acceleration sensors differ by…