Part Number: DRV10963 Hi team,
The datasheet mentioned that DRV10963P has blank OTP. However, the product page does not show DRV10963Pxx part number. Could you please let us know which one of below three is DRV10963P?
Best regards,
Kurumi
Part Number: DRV10963AEVM Other Parts Discussed in Thread: DRV10963 , USB2ANY Hi Everyone,
I have followed the section 5.4 of DRV10963 Evaluation Module User Guide at https://www.ti.com/lit/ug/slau643/slau643.pdf?ts=1592809456176&ref_url=https%253A%252F…
Part Number: DRV10963 Hello Support team,
DRV 10963 has OTP for several configurations. Is it only one chance to able to set the register for EVM?
According to Figure 19 in DRV10963 datasheet, the start-up time seems to take around 2s. Is it normal performance…
Part Number: DRV10963 Hi all Would you mind if we ask DRV10963? There is the description fFG_max (Hz) = 1300Hz on the datasheet P19. ->Therefore, is fFG_max (Hz) = 1300Hz fixed value? Is it possible to configure fFG_max (Hz) = 2000Hz? We would like to…
Part Number: DRV10963 Hi all Would you mind if we ask DRV10963? Could you let us know the background of "Default ILIMIT Soft current limit value=0.5A"? As our assumption; -Total Driver H+L Rdson Less than 1.5 Ω?(large Rdson?) -IOCP=1.8A, so…
Part Number: DRV10963 Hi Champion,
Some problems occurred when I use DRV10963 to drive my 5V-3phase BLCD motor. It turned out that no matter how I configured the parameters under the guidance of EVM’s user guide in DRV10963EVM GUI, my motor just failed…
Part Number: DRV10963 Hello everyone,
1. I want to use a Brushless 5V for a stirrer application and i want to use this driver : DRV10963. I tried to drive a quadricopter BLDC with it (rated 12V). I know that it's not rated for it but i just wanted to…
Part Number: DRV10963 Dear TI staff
I had posted such topic in October, 2016.
But I did not reply in that time because I had gone to short term internship.
Then I came back and reply one week ago.
So I re-post my topic for remind.
Please help me.
…