Part Number: DRV10983 Other Parts Discussed in Thread: , MCF8316C-Q1 Hi,
Comparing DRV10983 and DRV10983-Q1 I noticed that Phase-Phase inductance is specified different in the datasheet (0.7 mH DRV10983-Q1 Table 36 ; 0.07 mH DRV10983 Table 10).
We wo…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 , DRV10982-Q1 ,
How do I identify the DRV10983?
Typically an I2C device can be detected purely by it's presence at an I2C address (in a closed architecture). However, some devices can share…
Part Number: DRV10983-Q1 Hi Team,
1) Can the DRV10983Q1 set the PWM operating range? Now only the lowest duty cycle setting is seen, below 5% is output at 5% and below 1.5% is output at 0. Is there a maximum duty cycle setting that allows it to output…
Part Number: DRV10983-Q1 Dears,
1. Can DRV10983Q1 set the PWM working range? Currently, we only see the minimum duty cycle setting. If it is less than 5%, it will output 5%, and if it is less than 1.5%, it will output 0; Is there a maximum duty cycle…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 Hello experts,
Our customer encountered some problems when design DRV10983-Q1, can you help with it:
No
PN
Question describe
reply
1
DRV10983
When the LDO mode is selected…
Part Number: DRV10983-Q1 I wish to control four DRV10983-Q1 ICs with one controller using I2C interface. The DRV10983-Q1 device provides an I2C slave interface with slave address 101 0010. How can I change the address of individual DRV10983-Q1 so that …
Part Number: DRV10983-Q1 Please explain all the steps involved along with the exact software versions to be installed to run DRV109xx GUI on Windows 11.
Thank you.
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 I am using DRV10983 for ceiling fan application. I have tuned the motor and started running only in open loop. Motor is started with align method and smoothly starts, once the fan rpm goes…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: TIDA-01373 A little background on what has happened. I have been successfully using this driver to run a BLDC motor and control it's speed.
I was making adjustments to the configuration registers…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: MCF8316A Hi,
at the moment I'm doing some research for an application at which I need to fulfill the following points:
Controlling the output-shaft position with an accuracy approx. +/- 1…