Part Number: DRV2605L-Q1 Hi,
The customer wants to add a haptic function to the column SBW.
Is it possible to diagnose the OPEN SHORT status of the actuator only when it is active?
Part Number: DRV2605L-Q1 Hello, Please let me know what feedback you have on the following haptic driver. I believe they are the same device; I will be doing a review in parallel! Thanks, Nikola
Part Number: DRV2605L-Q1 Other Parts Discussed in Thread: DRV2605L Hi team,
Customer connect VDD to EN pins. When customer pull up SCL and SDA with 5V and VDD/EN don't have 5V input, customer found that there is around 5V at VDD/EN pin. Is that reasonable…
Part Number: DRV2605L-Q1 Other Parts Discussed in Thread: DRV2605L Dear TI engineer
This is Johnson.
Here are the questions about DRV2605-Q1
(1) If DRV2605-Q1 support Real time playback, what's the input frequency in I2C? And what tools I can use…
Part Number: DRV2605L-Q1 When I supply 3.3V to SDA/SCL pin, I can see that there is a leakage voltage close to 1V at VCC pin. Are they connected internally?
Part Number: DRV2605L-Q1 Hi, Team,
My customer have some questions about the DRV2605L-Q1, could you give some feedback?
1. When using the back-EMF voltage sensing to do the auto adjusting the drive frequency, how much time to do the adjusting?
2…
Part Number: DRV2605L-Q1 Dear TI engineer
This is Johnson.
Here are the questions about DRV2605-Q1
(1) If DRV2605-Q1 support Real time playback, what's the input frequency in I2C? And what tools I can use to tune the waveforms?
(2) I assume there…
Part Number: DRV2605L-Q1
Hi,
I have same problem.
when ı use ERM, DIAG_RESULT bit working correctly but if ı use LRA dont
I am taking "1" value from DIAG_RESULT bit after calibration mode and Diagnostic mode , always
LRA: DM LM1040F- A
0.6Vrms…