Part Number: DRV2625EVM-MINI Other Parts Discussed in Thread: DRV2625 , DRV2667 I have PeizoHapt module - PHUA3015-30A-21-000 with me, SO I just wanted to know whether using DRV2625EVM-MINI I can control PeizoHapt module. If yes, then I should go with I2C…
Part Number: DRV2625 Other Parts Discussed in Thread: USB2ANY , Hi Team,
I bought DRV2625EVM-MINI and USB2ANY for LRA drive.
When using the DRV2625EVM-MINI with USB2ANY, which version should I use with the firmware of USB2ANY? VDD(=3.3V) was not output,…
Hi Christine.
Thank you. Please let me ask some questions again.
Do I have to edit the source code of the DRV2625EVM-CT in the way described in the "Modifying or Reprogramming the Firmware" section of the datasheet?
Am I correct in assuming that…
Part Number: DRV2625 Hey,
I am Evaluating DRV2625EVM-MINI Evaluation Board with an Linear Resonant Actuator whish spécification are:
-Vibration-Frecency: 2.5Grms@100Hz(Fact)
-Thermal Resistance: 15.3Ω
-Power Consumption: <300mW @2.23Vrms…
Hi Jackson,
You can connect an external I2C source to J4, as long as it is referenced to the same potential (3.3V).
Although this EVM is mainly purposed to be controlled by on-board MSP through Haptic Control Console software, thus the on-board actuator…
Part Number: DRV2625 Hi,
We are evaluating the DRV2625 using the DRV2625EVM-MINI evaluation board. In our initial test setup, we were encountering under-voltage errors until we increased the capacitance for C(vdd) input capacitor, which resolved the problem…
Part Number: DRV2605L Other Parts Discussed in Thread: DRV2625EVM-CT , DRV2605EVM-CT , DRV2625 , DRV2625EVM-MINI The TI site says the Hap-Touch boosterpak is still available at Newark but they don't list it.
Not on TI store as it goes to Newark for the…
Other Parts Discussed in Thread: DRV2604 , DRV2605 , DRV8601 , DRV2625EVM-CT , DRV2605EVM-CT , DRV2625 , DRV2625EVM-MINI I need use DRV2605 , DRV2604 or DRV8601 to drive the LRA which used in some phones like S6/S7 or note . I need a circuit or pcb to make it…