Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: DRV2700 Hi, I'm Jeon Hyeon Min.
I'm using DRV2700EVM-HV500 for driving piezoelectric actuator.
What I want is 0~158V AC sine wave output for 0~200Hz using DRV2700EVM-HV500.
So I found…
Part Number: DRV2700EVM-HV500 Hello, I'm Jeon Hyeon Min
Although I read DRV2700EVM-HV500 User's guide so many time, I don't understand how to use DRV2700EVM-HV500.
Here's my questions.
1. I'm using piezoelectric actuator which has 0.8…
Part Number: DRV2700EVM-HV500 Hello,
New and not know much about of Piezos, but I have DRV2700EVM-HV500 and got few piezocermic trimorph bending actuator. So can I drive bender with this evaluation board? Bender guide says "It is suggested to use a series…
Hi Bruno,
If the piezo is operating differently between the two, then the two output signals must be different. An oscilloscope screen shot would really help debug this issue. Without it, there isn't much I can do.
Regarding the noise, you are operating…
Part Number: DRV2700EVM-HV500 Hello, My customer has a DRV2700EVM-HV500 but does not currently have a piezo element to connect. It seems that it will take a long time to acquire a piezo element. They want to evaluate the DRV2700EVM-HV500 output by connecting…
Part Number: DRV2700EVM-HV500 Hello,
i have bought drv2700evm-hv500 board,
i conncetd the piezo injector and testing it,
i want to actuate it faster , for example at 150hz frequncy, with 1ms on and rest off.
it is possible to achive with this board, if…
Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: DAC63204 , Hi all, Currently I am using DRV2700EVM-HV500. I need to drive a piezo actuator (350nF) from 0 to 150VDC. I am using DAC63204 as my analog input. I already set my EVM boost voltage…
Part Number: DRV2700EVM-HV500 Hello,
i need help with actuating the piezo injectors which has capacitance of 1uf and resistance of 200k ohms. can anyone tell me does drv2700evm-hv500 able to actuate it. if not which is the suitable ic.
i dont have exact…
Part Number: DRV2700 Other Parts Discussed in Thread: DRV8662 , , Hello,
I could not find any information related to safety and isolation of the DRV2700 chip or its equivalent the DRV8662. We have been working so far with the DRV2700EVM-HV500 modified to…
Part Number: DRV2700EVM-HV500 I'm running windows 10 and trying to connect to my DRV2700EVM-HV500 but the device is not recognized by piezo control console. When I try to follow the firmware update/scan device procedure the board doesn't show up, I just…