Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5013 Hello Team,
I got a question from customer about the DRV5013-Q1.
Q. Does DRV5013-q1 have internal clock? If yes, Do you know the frequency?
Customer want to know whether the clock…
Part Number: DRV5013-Q1 Hi,Staff
Please tell me how to calculate Vol (Output Loe Level voltage). I'm thinking of the following calculation, is there any problem?
Vcc=5V, Output-Pull up =1kΩ, Rds=50Ω
Vol = 5V/(1kΩ + 50Ω)×50Ω = 238mV(min) Vol = 5V…
Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5013 Hi,
I wanted to implement two Output capacitors at the output pin of DR5013-Q1 as shown in the Figure attached. I am implementing those due to checking of Conducted susceptibility at…
Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5013 Dear, Sir.
tON typical & maximum values are defined on the datasheet, page 6.
My customer is asking the duratuion of ON=Low after power-up.
Is it possible to clarify & assure about…
Part Number: DRV5013-Q1 Hello,
a customer would like ot know the maximum thermal load capacitance of P/N: DRV5013ADEDBZRQ1.
Can you please advise?
Thank you very much.
Best regards
Adnan
Part Number: DRV5013-Q1 Is there any DRV5xxx hall sensor working at 180 degree ambient operating temp? the application is for the servo motor.
It seems the E version can work up to 150degree only.
Regards
Brian
Part Number: DRV5013-Q1 Dear, Sir.
My customer is asking about the output when VCC is under 2.5V.
VCC range is defined from 2.7V to 38V.
According the datasheet description, I am gussing it would be Hi-Z?
Sorry to ask about this kind of matter…
Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5055 Dear Community
Use the Hall sensor to measure the angle of the DC motor. The measurement error is a requirement of ±1°. Do you have a Hall sensor that satisfies this?
Thanks.
Part Number: DRV5013-Q1 Hi Sir,
Per tidu835, pls give some advice about the distance between the magnet and sensor? or pls tell us the distance in this reference. The magnet used in this design, how much is the magnetic strength?
Part Number: DRV5013-Q1 Hi
What is the maximum value of Tr and Tf at pin "OUT" of DRV5013-Q1?
In the datasheet of the device, the tyipcal value is 200ns as Tr and 31ns as Tf. PLS let me know the maximum value at the same test condtions as shown in…