Part Number: DRV5055 Other Parts Discussed in Thread: CC1352R hello everyone
can anyone explain how drv5055 hall effect sensor sense current in the wire or it just sense the breakout of wire ?
there is some terms given like "output voltage to stay within…
Part Number: DRV5055
Hello I have a question about the current consumption of DRV5055A2QLPGM. The current consumption is 6 to 10 mA in the data sheet before December 2023. The data sheet was revised in December 2023, and the current consumption has been…
Part Number: DRV5055 Greetings,
I have an application where I need to measure precisely the magnetic field with several linear hall effect sensors. Is it possible to get a bunch of linear Hall effect sensor with the same sensitivity to eliminate the 5…
Part Number: DRV5055 I have a question regarding the error in sensor sensitivity of DRV5055.
For the Z4 type, it is stated that when using a power supply of 3.3V, the sensitivity will be in the range of 7.1mV/mT (min) to 7.9mV/mT (max).
Does the stated…
Part Number: DRV5055 I have two questions regarding the statement that the sensor linearity error of the DRV5055 is approximately ±1%. 1.This states that linearity error is defined as the difference in sensitivity between any two positive B values…
Part Number: DRV5055-Q1 Hi,
We are trying to use Hall sensor(DRV5055A1ELPGMQ1) for measuring the magnetic field intensity of a electromagnetic (12V KK-P20/15).
Can anyone help how to place hall sensor.
As per data sheet hall sensor output voltage should…
Part Number: DRV5055 Hi team,
Is there any introduction material for SNR measurement for hall IC?
Should we put a termination or buffer at the output when we measure the SNR of DRV5055?
Regards,
Thank You Scott Bryson,
1. Actually I am looking for DRV5055 sensor placement, like below image
So the size of magnet should be such that the flux are within 168mT at < 0.5mm distance.
Same criteria we can assume material as N42 & SmCo24 with inner…