Part Number: DRV5055-Q1 Other Parts Discussed in Thread: DRV5055 So, I need to simulate sensor the part number is, DRV5055 which linear hall effect sensor. which tool can I used to simulate the sensor.
Part Number: DRV5055-Q1 Other Parts Discussed in Thread: DRV5055 DRV5055A2ELPGQ is AEC-Q100 Grade 0. I would like to ask the question below :
Is this PEM (PLASTIC ENCAPSULATED MICROCIRCUITS) part?
What condition that TI use for HTRB or HTOL (High Temperature…
Part Number: DRV5055-Q1 Hi,
We are trying to use Hall sensor(DRV5055A1ELPGMQ1) for measuring the magnetic field intensity of a electromagnetic (12V KK-P20/15).
Can anyone help how to place hall sensor.
As per data sheet hall sensor output voltage should…
Part Number: DRV5055-Q1 Hi team,
Hope you are doing good.
Do we have any recomended pcb layout for this sensor? If there is any can you share the details with us.
Regards
Vivek Gandham.
Part Number: DRV5055-Q1 Other Parts Discussed in Thread: DRV5055 , TMAG5170
Is DRV5055 capable of sensing changing magnetic field at 10000rpm motor speed, if the magnetic field is within the sensor limit?
The sensor is linear in nature, whereas its application…
Part Number: DRV5055-Q1 Have a few questions in regards to a TI calculator I am using, Magnetic Sensing Proximity Tool. When I change the type of magnet from block to cylinder the data gets weird, is that correct?
Part Number: DRV5055-Q1 Other Parts Discussed in Thread: DRV5055 Hi team,
could you help tp check
What is the drive current of the Driver and can it be connected directly to the ADC? thanks
Part Number: DRV5055-Q1 We are using Analog hall sensor for position measurement and would like to calculate the worst case variation in Voltage output with respect to Magnet distance from hall sensor .
Magnet Gauss Value : Minimum 4430G , Typical 4365G…
Part Number: DRV5055-Q1 Hello,
We urgently need the HTOL data for this Grade 0 automotive part. The qualification data says " Per grade requirements. See data sheet." Since this is a Grade 0 part, my assumption is that HTOL was performed for…
Part Number: DRV5055-Q1 Other Parts Discussed in Thread: DRV5055 My customer is adding a pullup resistor to the output of DRV5055-Q1 as recommended in the datasheet (Figure 20). They want to know what is the output resistance value (Rout) of the output…