Part Number: DRV8256 Hi Team,
The customer uses DRV8256PRGER to drive the DC brushed motor, and the power supply voltage is 24V. In the case of not driving the motor, the DRV8256PRGER chip generates severe heat, but it functions normally. The following…
Part Number: DRV8256 Hello Expert, I have question regarding use case of this device. Our customer looking for chopping current limit time load switch from the point of view of heat-up. As far as our confirmation, there isn't such at load switch but some…
Part Number: DRV8256 Hello We are using DRV8256E to drive one of the valve (uses DC Motor). There are 4 such valves in system, all of them driven by above HBridge
Interestingly the valves that are away (physically) from HBridge circuit operate without…
Part Number: DRV8256 Hi, TI expert.
The customer has applied the DRV8256ERGER and has the following defect during the test.
--------------------------------------------------------------------------------------------------------------------------…
Part Number: DRV8256 Hi sir,
The datasheet of the product mentions a 5A peak current while the webpage mentions 8A. Which one is the correct value? Also is there any information available about maximum continuous current? The datasheet isn't clear to…
Part Number: DRV8256
Hi Team,
Developing a board in which a connector a pin shares the half bridge output of the DRV8256P with an open collector input, as shown in the following diagram:
The idea was to configure the board in two ways: Configuration…
Part Number: DRV8256 Hi teams:
When the 8256e is set in the fast decay mode, is there any output only when the input PWM duty cycle is within 50% - 100%?
Part Number: DRV8256 Other Parts Discussed in Thread: DRV8840 , Issue:
The DRV8256EPWER does not implement the DECAY function even though it has the DECAY pin, the detailed information of pin as follows:
But DRV8840 has the SLOW DECAY function…
Part Number: DRV8256 Other Parts Discussed in Thread: DRV8426 , Hi Expert,
I cannot find the description about how to set Ivalley value in datasheet.
Could you please let me know it?
datasheet
Smart tune Ripple Control operates by setting…