Ram babu said: Post following these steps, I could not see any waveform in the graph window.
Run the lab to spin the motor and click the continuous refresh on the graph tool window.
Ram babu said: In addition to the problem above, I have 1 query. What is…
Part Number: DRV8301-69M-KIT Hello There,
I am running DRV830x-HC-C2-KIT with INSTASPIN-FOC GUI
IN the GUI when we click on " Identify the motor parameter" button , then GUI is showing DRV fault status RED and Reset DRV fault is not working.
I have…
Part Number: DRV8301-HC-C2-KIT Hi
we are looking for a suggestion on sinusoidal control BLDC motor with resolver/encoder part which is compatible with DRV8301-HC-C2-KIT.
on specification:
Maximum rated voltage: 28 Volts
speed: 5000 rpm
we are looking for…
Part Number: DRV3255-Q1 Other Parts Discussed in Thread: DRV8301 , Hello There,
I am using this DRV830x-HC-C2-KIT . I want to change DRV8301 to DRV83255-Q1.
I have two query :
1.what is key difference between DRV3255-Q1 and DRV8301.
2.what is the correct…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: MOTORWARE Hello TI Team,
We are using proj_lab05b of the motorware for F28069M Kit.
I want to know the following things related to the usage of the project.
1. While importing the project…
Other Parts Discussed in Thread: CONTROLSUITE , INSTASPIN-BLDC “DRV830x-HC-C2-KIT”
Control Mode :Allows the selection of four different control modes
Duty Cycle: The motor is commutated using the sensorless algorithm but is driven in an open…
Part Number: DRV8301-HC-C2-KIT Dear All i am using the Project provided in control suit to run a motor currently the motor runs fine if i am running the same with NO Load it statrts and Atains it maximum RPM but when i connect the same with Load the more…
Part Number: DRV8301-HC-C2-KIT Hi team,
Here're some problems from the customer may need your help:
In the schematic in the above path, the current acquisition circuit for the bus bar is designed as follows:
The amplification circuit is 30…
Part Number: DRV8301-HC-C2-KIT Hi team,
Here're some problems from the customer may need your help:
The PM_Sensorless routine in the DRV830x-HC-C2-Kit_v105 development package for TI\controlSUITE\development_kits.
In this routine, the driver board…