Ram babu said: Post following these steps, I could not see any waveform in the graph window.
Run the lab to spin the motor and click the continuous refresh on the graph tool window.
Ram babu said: In addition to the problem above, I have 1 query. What is…
Part Number: DRV8301-69M-KIT Hello There,
I am running DRV830x-HC-C2-KIT with INSTASPIN-FOC GUI
IN the GUI when we click on " Identify the motor parameter" button , then GUI is showing DRV fault status RED and Reset DRV fault is not working.
I have…
Part Number: DRV8301-HC-C2-KIT Hi
we are looking for a suggestion on sinusoidal control BLDC motor with resolver/encoder part which is compatible with DRV8301-HC-C2-KIT.
on specification:
Maximum rated voltage: 28 Volts
speed: 5000 rpm
we are looking for…
Part Number: DRV3255-Q1 Other Parts Discussed in Thread: DRV8301 , Hello There,
I am using this DRV830x-HC-C2-KIT . I want to change DRV8301 to DRV83255-Q1.
I have two query :
1.what is key difference between DRV3255-Q1 and DRV8301.
2.what is the correct…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: MOTORWARE Hello TI Team,
We are using proj_lab05b of the motorware for F28069M Kit.
I want to know the following things related to the usage of the project.
1. While importing the project…
Other Parts Discussed in Thread: CONTROLSUITE , INSTASPIN-BLDC “DRV830x-HC-C2-KIT”
Control Mode :Allows the selection of four different control modes
Duty Cycle: The motor is commutated using the sensorless algorithm but is driven in an open…
Part Number: DRV8301-HC-C2-KIT Dear All i am using the Project provided in control suit to run a motor currently the motor runs fine if i am running the same with NO Load it statrts and Atains it maximum RPM but when i connect the same with Load the more…
Part Number: DRV8301-HC-C2-KIT
Hello,
I found a mistake in the InstaSPIN_BLDC source code related to GPIO pin configuration.
This is actually to do with the config of the Hall Input pins which are unused for the entirety of the 'Quickstart Guide'…
Part Number: DRV8301-HC-C2-KIT Hi team,
Here're some problems from the customer may need your help:
In the schematic in the above path, the current acquisition circuit for the bus bar is designed as follows:
The amplification circuit is 30…