Hi Ram,
Do you still require further assistance on this? Please help mark the thread as resolved if there are no further questions. Thanks.
Best Regards, Andrew
Part Number: DRV8301-69M-KIT Hello There,
I am running DRV830x-HC-C2-KIT with INSTASPIN-FOC GUI
IN the GUI when we click on " Identify the motor parameter" button , then GUI is showing DRV fault status RED and Reset DRV fault is not working.
I have…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: MOTORWARE Hello There,
I am running DRV830x-HC-C2-KIT with INSTASPIN-FOC GUI.
I have following questions regarding the motorware_1_01_00_18 Lab solutions: \ti\motorware\motorware_1_01_00_18\docs…
Other Parts Discussed in Thread: CONTROLSUITE , INSTASPIN-BLDC “DRV830x-HC-C2-KIT”
Control Mode :Allows the selection of four different control modes
Duty Cycle: The motor is commutated using the sensorless algorithm but is driven in an open…
Part Number: DRV8301-HC-C2-KIT Hi
we are looking for a suggestion on sinusoidal control BLDC motor with resolver/encoder part which is compatible with DRV8301-HC-C2-KIT.
on specification:
Maximum rated voltage: 28 Volts
speed: 5000 rpm
we are looking for…
Part Number: DRV8302-HC-C2-KIT Hello Guys,
Good day.
In the DRV8302-HC-C2-KIT BOM file, a 140 mohms inductor rated at 1.5A were mentioned (DR74-330-R). However this Inductor is currently not available in the market. Is it okay to replace it with a 130 mOhms…
Part Number: DRV8301-HC-C2-KIT
Hello,
I found a mistake in the InstaSPIN_BLDC source code related to GPIO pin configuration.
This is actually to do with the config of the Hall Input pins which are unused for the entirety of the 'Quickstart Guide'…
Part Number: DRV8301-HC-C2-KIT Dear All i am using the Project provided in control suit to run a motor currently the motor runs fine if i am running the same with NO Load it statrts and Atains it maximum RPM but when i connect the same with Load the more…