Part Number: DRV8305-Q1EVM Other Parts Discussed in Thread: DRV8305-Q1 , MOTORWARE , CCSTUDIO Hi,
We are using DRV8305-Q1 EVM to run a BLDC motor. I have used the following steps
1) J3 jumper is changed to USB and loaded the code using micro-USB and CCS.…
Part Number: DRV8305-Q1 Other Parts Discussed in Thread: DRV8305 Hi
We should make an A-sample. This should power two coils for two valves.
We already developed a small motor application for his customer with the DRV8305. We should also keep this driver…
Part Number: DRV8305-Q1 Other Parts Discussed in Thread: DRV3245Q-Q1 Hi,
We need functional safety data FIT rate etc. for DRV8305-Q1 gate driver.
Can anyone provide.
Our application is ASIL B, BLDC motor controller.
Regards,
Abhishek D.
Part Number: DRV8305-Q1 Other Parts Discussed in Thread: DRV8305 Customer was designing DRV8305-Q1 for the sensorless BLDC with FOC control, together with MSPM0G MCU. They did not have experience on DRV and M0. Could you please help provide the example…
Hi Kura,
kura said: they just wanted to know that there was no problem with their usage and that it was operating within specification.
The spiking on PVDD that they are seeing should not cause any problem to the device or its operation. Also, even with…
Part Number: DRV8305-Q1 Hi~ All
Designed DRV8305-Q1 and AVDD failure happen..
Datasheet recommend 1uF output cap for AVDD, but customer used 4.7uF from previous design(DRV3245-Q1 circuit.)
Please, refer failure symptom and let me have feedback for…
Part Number: DRV8305-Q1 Other Parts Discussed in Thread: DRV8305 Hello All, I am trying to simulate a motor driver in MATLAB Simscape and want to add the DRV8305 model to my project. I have attempted importing using the SPICE model listed under the link…
Part Number: DRV8305-Q1 hi expert
For ULVO function in datasheet, i have two questions
Q1: How can i understand the parameter of PVDD falling and PVDD rising?
Let us assume PVDD is 10V now, when PVDD is rising to 42.5V(10V+32.5V( shown in datasheet )) because…
Part Number: DRV8305-Q1 Other Parts Discussed in Thread: DRV8305 Hello,
we are using the DRV8305NQPHPQ1 as the gate driver for our BLDC motor control board and are experiencing a jump in the the total current to the board from 70 mA to 390 mA when the…