Part Number: DRV8308 Each SUB board and main board has an MCU. The SUB board has DRV8308 and MCU#2, and the main board has MCU#1.
MCU#2 on the SUB board is connected to DRV8308 via SPI and is only responsible for the initial setup.
MCU #1 on the main…
Part Number: DRV8308 Other Parts Discussed in Thread: CSD88537ND Hi, TI expert
The customer is using ITOH DENKI's motor controller (see attached file below), but we are developing a new motor controller with the same performance as some functions are…
Part Number: DRV8308 Tool/software: Dear TI Support Team,
I am using the DRV8308 driver with the MFA0500 high-speed blower (by Airfan) . I have successfully verified that the motor operates correctly in open-loop mode using the DRV8308. However, I am…
Part Number: DRV8308 Tool/software: Hi,
Iam Driving the AIRFAN MFA0500 Blower (one-pole pair) using Drv8308,using STM32 Controller. Clock PWM Method is used for speed control Input.MFA0500 Speed range max 80000 rpm, peak current is 4.75 A .
1. Using…
Part Number: DRV8308 Tool/software: Hi Team,
Nice to meet you
My customer is looking for BLDC motor driver IC.
The application is a conveyor belt. And they are using PM500FE motor. So they are developing PM500FE motor controller.
the following…
Part Number: DRV8308 Tool/software: Hi all,
I'm developing a motor control circuit using DRV8308 now.
There is a description as follows in section 7.3.7 in the datasheet. ****************************** If BRKMOD= 0, the outputs are 3-stated, resulting…
Part Number: DRV8308 Tool/software: Hi Team,
I'd like to request you the output stage circuit design review. Please check the attachment below and let me know the recommended resistor values of R8, R9 and overall review result.
Output stage circuit…
Part Number: DRV8308 Other Parts Discussed in Thread: CSD88537ND Tool/software: Hello there!
I'm working on the controlling of MFA0500 Airfan Turbine using DRV8308 BLDC motor Driver, my turbine motor is a one pole pair and Max. rpm is 73000 and Peak…
Part Number: DRV8308
Tool/software:
Hi I'm trying to communicate with drv8308 through ssi but its reading 0xFF every time.
#include <stdbool.h> #include <stdint.h> #include <stdio.h> #include <string.h> #include "inc/hw_i2c.h" #include "inc/hw_memmap…
Part Number: DRV8308 Other Parts Discussed in Thread: MCT8329A Hi Team,
The DRV8308 controller implements closed-loop speed control, allowing the motor to run at a precise speed over a wide load torque range. It's required 100W of power to drive motors…