Part Number: DRV8312-C2-KIT Good Evening all
I am trying to control the speed of a Small BLDC motor using the pot provided in the DRV8312 EVM , i am using F28035 control card and i currently running the BLDC_Sensor less code. My ADC is working fine and…
Part Number: DRV8301-HC-C2-KIT Hi
we are looking for a suggestion on sinusoidal control BLDC motor with resolver/encoder part which is compatible with DRV8301-HC-C2-KIT.
on specification:
Maximum rated voltage: 28 Volts
speed: 5000 rpm
we are looking for…
Dear Sir/Madam,
We are currently working on a project regarding position control of a positioning stage based on a parallel kinematic mechanism. Here three linear Airex BLDC motors need to be controlled via servo-loop. First, we are
planning to control…
Part Number: DRV8312-C2-KIT Good morning,
I've encountered a problem when i run instaspin lab12a sensored on DRV8312-C2-KIT with F28069 microcontroller.
When i try to start the motor, it not runs.
I'm using a motor that use 3 Hall sensor and not an…
Part Number: DRV8312-C2-KIT On lab11e i have the same problem report by the the linked question.
When i run lab11e to test a smooth transition between hall sensor control(at low speed) and sensorless instaspin fast control (at high speed), the motor behaviour…
Part Number: DRV8312-C2-KIT Hi I am currently working with NEMA 17 55W BLDC motor comes with DRV8312 C2 kit. I want to know how much voltage I needed to give to the motor hall sensor wires to only turn on its hall sensor? I want to see hall signals coming…
Part Number: DRV8312-C2-KIT Good morning,
i'm working on instaspin foc.
i executed lab04 (Torque mode controller) and the following labs that execute the Speed mode Controller.
I want to know if is it possible to skip from a controller mode to another…
Part Number: DRV8312-C2-KIT Tool/software: TI C/C++ Compiler Hello,
we have a DRV8312-69M-KIT (2019) and for that we have installed and configured to work properly, MatLab 2019a, CCS 6.2 and UniFlash 4.1. Taking the example c28069pmsmfoc_ert.slx and building…
Part Number: DRV8301-HC-C2-KIT Dear All i am using the Project provided in control suit to run a motor currently the motor runs fine if i am running the same with NO Load it statrts and Atains it maximum RPM but when i connect the same with Load the more…
Part Number: DRV8301-HC-C2-KIT Hi team,
Here're some problems from the customer may need your help:
The PM_Sensorless routine in the DRV830x-HC-C2-Kit_v105 development package for TI\controlSUITE\development_kits.
In this routine, the driver board…