Part Number: DRV8320 Other Parts Discussed in Thread: DRV8303 , Hello Expert,
We have to change from DRV8303(HTSSOP) to DRV8320S (WQFN) because of package size issue.
We are using external ADC ∑△. This device requires VDD1 pin floating power.
So when…
Part Number: DRV8320 Hi team,
My customer is going to use this device in a stepper. The stepper is a Lens drive motor inside automotive lidar.
They will only use two half bridge. Is it OK? Is there any other customer use like that?
Part Number: DRV8320 Hi Team,
42V supplies power to 8320H. When DRV8320H simulates a high side MOS short circuit on the upper tube, it triggers the hot circuit protection and 8320H enters nsleep mode.
At this time, most of the functions of the driver…
Hello Zhipeng,
Have you been able to resolve your issue? If so please press the "This resolved my issue" button to any of the answers.
If you have any other additional questions please feel free to post another E2E question, other wise I will…
Part Number: DRV8320 Hi,
is 1x mode applicable for sensoreless motor operation?
if it is , how to run sensoreless motor with using external microcontroller.
Part Number: DRV8320
Hi Team,
The motor has leakage problems, with very large spurs at the drive end and erratic spurs, causing the motor to spin abnormally.
(The Chinese in above figure is, "PCB copper thickness is 1 oz., temperature rise is 20 degrees…
ÖMER FARUK YÜMNÜ said: We can change the direction using this pin, but what I want is to change the direction just by changing the phases. is there a way to do this ??
I was wrong previously saying you could change the phase wiring to reverse motor direction…
Part Number: DRV8320 Would you provide a non-encrypted Pspice model of DRV8320 ?
I'm troubled now that I cannot import the encrypted model into EMC simulation tools that's not Pspice itself.
Part Number: DRV8350 Other Parts Discussed in Thread: DRV8320 ,
Hello
I am looking to replace DRV8320 With DRV8350 .
Are the materials of the terminals and the internal structure(e.g. wire bonding ,leadframe etc) same?
I am concerned about the effect…