Hi Jan,
That's great to hear you were able to find the root of your issue, please feel free to post another E2E if you still have issues.
Regards,
Yara
Hi Annie,
I apologize for the delay.
After further overview it may be that the device CSA shunt configuration is causing the VDS monitoring to trip.
For this single shunt CSA configuration, I believe only one amplifier should be connected and the other…
Hi Abhijeet,
It looks like you already have a thread open regarding this question.
https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1331032/drv8323-hard-lock-jam-bldc-at-0-speed-motor-using-drv8323
I'm closing this…
Part Number: DRV8323 Dear Sir dear MS
I am implementing a new new motor driver section.
Currently I have the following requirements:
24V, 1A, 2A max / fault.
The power stage uses BUK6D56-60E. These transistors have a total gate charge of 7.5nC
From my…
Part Number: DRV8323 I am driving bldc motor using drv8323 motor driver in 1xPWM mode. I want my bldc motor to get hard locked or jammed at 0 speed. The motor should not rotate even if we try to rotate it through physical force. I used INLC pin but that…
Part Number: DRV8323 There appears to be an error in the DRV8323 datasheet. Sections 9.2.1.2.4 and 9.2.2.2.1 Equations 23 and 28 appear incorrect because they state that the gain must be greater than max voltage/(sense resistor * max current). I believe…
Part Number: DRV8323 Hello,
please provide the correct/latest datasheet for DRV8323SRTAR. Now I get two different datasheets with two different MSL values 1 & 2, please check the links below. also on the website is set as 1
https://www.ti.com/lit/ds…
Part Number: DRV8323 Hi
A circuit is being designed to read the FET current value using the Current Sense Amplifier within the DRV8323HS. We are going to use 5V/V gain and want to limit bandwidth by applying RC primary LPF to SOx which is sensor output…