Part Number: BOOSTXL-DRV8323RS Other Parts Discussed in Thread: MSP-EXP430F5529LP , DRV8323 , MCT8316Z Hello,
I'm looking for a way to use the BOOSTXL-DRV8323RS at a constant speed with varying loads. The BOOSXL_DRB823X GUI used with the MSP-EXP430F5529LP…
Part Number: BOOSTXL-DRV8323RS Hi Team,
The customer wants to know whether it is feasible to add inductors to the three phases of the brushless DC motor to reduce the slope and amplitude of the drive current, thereby reducing the temperature rise of the…
Part Number: BOOSTXL-DRV8323RH Hi,
Can you please help to confirm if little resistor e.g. 10 ohm is needed in GH and GL line to prevent oscillation damage MOSFET ?
also for the resistor C1, is it connect to board GROUND or to MOSFET's SOURCE ? such as…
Part Number: DRV8323R I am using drv8323rs partnumber. Due to a design mistake, I did not include the DVDD's decoupling capacitor in the artwork. At this time, when operating the motor, an unknown offset was detected in the motor current depending on…
Part Number: BOOSTXL-DRV8323RS While spinning a BDLC motor in 1x PWM mode, I keep getting a "VOLTAGE" fault in the GUI window (where the speed and direction is set), which causes the motor to stop. To be clear, this is NOT an Overvoltage, Undervoltage…
Part Number: LAUNCHXL-F280039C Hi team,
I can't select "DRV8323RS" in UMCL syscfg. Also I can't choose "2" at Number of Motors. Is something wrong?
・Board :LAUNCHXL-F280039C
・Motor Driver :DRV8323RS-EVM
・control method :FOC…
Part Number: DRV8323R Other Parts Discussed in Thread: DRV8353 Hi support team.
My customer is considering BLDC motor system with sinusoidal control by using hall sensor.
They asked us about sinusoidal drive with DRV8323R on 1xPWM mode.
Is it possible…
Part Number: BOOSTXL-DRV8323RS Hi Team,
Customer just connects the BOOSTXL-DRV8323RS evaluation board to the BLDC motor without connecting the MCU. Could he make the motor rotate by rotating the encoder in the picture?
Regards,
Annie