Hi Jason,
Thanks a lot for your response. After doing the changes suggested by you, there is significant reduction in throttle response time.
Regards,
Premkumar T.
Part Number: DRV8353RS-EVM
Hi,
I am using the DRV8353RS-EVM to operate the BLDC motor, and I am controlling the motor speed using the GUI. I pressed the RESET switch S2 (FSMJSMA), and the EVM board began signalling the fault. I then tried to connect…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 Hello Team,
I am working on DRV8353 with F280015x interfacing with 48V PMSM Motor with Hall feedback . At no load conduction Motor is working fine, motor all 3-phase current are same.
A…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 Hello Team,
I am working on DRV8353 with F280015x interfacing with 48V ABZ+PWM Motor. On the UMC code I enabled the ABZ ENC feedback by enabling the "MOTOR1_ENC" macros for enabling the…
Part Number: DRV8353RS-EVM
Hi,
Please help for below queries.
1.
We don't want to use shunt resistor for motor phase sensing.
Instead of shunt resistors we are using hall sensor for motor phase sensing. - See Below reference image
Can we connect…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 Dear Sir/ Madam,
I am looking for DRV8353RS spice model. It would be really helpful if you can please share.
Thanks and regards,
Poojitha.
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: MOTORWARE , DRV8353
Previously, the online GUI was not linked, so we are proceeding it again through motorware. The current progress is as follows.
We are following the SLVUBH8B guide. 1. Installation…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: MOTORWARE , CCSTUDIO Currently, DRV8353RS-EVM kit is purchased and used. I followed the guide and installed MotorWare and UNIVERSAL GUI. All the copy paths in the guide were executed without any…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: MOTORWARE , DRV8353 , CCSTUDIO
Currently, DRV-8353RS-EVM kit is purchased and used. Follow the guide to.
slvu791b - Download and install the Setup_DRV8353Rx-1.0.0_EVM.zip file in accordance with…
Part Number: DRV8353RS-EVM Hello Team
I am using hall feedback and a 48V PMSM motor. The motor is operating noiselessly and smoothly.
How to operate the motor so that it runs smoothly. What motor parameter settings need to be set up?
Best Regards,
…