Part Number: DRV8434 Hello,
it is actually about the DRV8432 , but this can no longer be selected in the "Part Number" field. According to PDN# 20231002000.3, DRV8432 has an LTB of Oct 2024. It can no longer be found on the homepage. However, this…
Part Number: DRV8962 Hey Team,
I have a customer who is interested in the DRV8962DDVR device, and I saw that you are hoping to release it by March 20th. He was also curious as to why the DRV8432 was discontinued. If possible, could you tell me why?
Best…
Zoomed waves have been uploaded below.
As you known, we have used thermal pad between DRV8432 hot slug and heat sink in the current design. now we have removed the thermal pad and directly installed heat sink on DRV8432 with optimized stand off height…
Part Number: DRV8412 Other Parts Discussed in Thread: DRV8462 , DRV8262 , DRV8962
As DRV8432 moves into the end of its life the next step is to choose an alternative part. This device had a broad application base in medical devices, portable electronics…
Part Number: DRV8432 Hello.
I designed a circuit that drives Peltier using drv8432.
Try to control two peltiers with one drv8432
The circuit is...
GVDD=VDD=PVDD = 12V, (load = peltier) duty30%
(yellow = out_a port , blue = out_b port)
GVDD=VDD=12V…
Part Number: DRV8412 Other Parts Discussed in Thread: DRV8962 I have a design with DRV8432 devices on it, the design has been in the field for while. Could could I enquire when the EOL notice for the DRV8432 was issued? I didn't see it a year ago when…
Part Number: DRV8412 We are currently using DRV8432 to drive TEC . Thermoelectric cooler. The application notes recommend to use a low pass filter, I would like to know if the reference schematic given in page 22 of the datasheet is correct one. During…
Part Number: DRV8462 Other Parts Discussed in Thread: DRV8962 Is DRV8462 a replacement option for DRV8432?
I feel since DRV8462 is an exclusive stepper motor driver, it wouldn’t work well for Brushed DC motor control. Is this correct?
Thanks, …