Part Number: DRV8702-Q1EVM Other Parts Discussed in Thread: DRV8962 , DRV8262 Hi team,
I am testing DRV8702 evm with Eload.. I use PH/EN mode, the duty circle of PWM is 100%. PVDD is 6.2V from buck-boost controller. the load is about 1.14ohm. When driving…
Part Number: DRV8702-Q1EVM Newly purchased DRV8702-Q1EVM output is always 0v irrspective of PWM set via TI application.
Please provide the detailed steps/instructions to operate the eval kit.
user manual does not have proper information.
Part Number: DRV8702-Q1EVM Other Parts Discussed in Thread: DRV8702-Q1 I'm thinking getting a few of these boards to control electric motors in the vehicle using Arduino Mega, is it possible to do so? Is there any pin out on the board to control speed…
Part Number: DRV8702-Q1EVM Other Parts Discussed in Thread: DRV8702-Q1 , Hi team,
Recently I study the DRV8702-Q1 and make an experiment that use the DRV8702-Q1EVM to drive a brush motor, then I have some questions as follows,
1. ch1: pin-IN1/PH, ch2: pin…
Hi Mike,
Thank you for your answer,
There is no GUI Setup .exe provided on the DRV8702-Q1EVM Software (Rev. A) zip file, the only executable inside are CDM v2.10.00 WHQL Certified.exe and DRV8701EVM_GUIv1.0.exe .
I am running on windows 7 64 bits.
Regards…
Hello,
I have find out this following EVM boards & read all the document files related to this boards so out of all boards I can see input voltage range or Operating Voltage Range of this boards but in that document files I'm not able to find that EVM…
Part Number: DRV8702-Q1 Hello,
I'm trying to control LLC tank with full bridge MOSFET DRV8702-Q1EVM. LLC tank is connected betwen pins SH1 and SH2. I'm using other MCU with two PWM channels.
The only things have issue is with measuring the current…
Hello Simone, The USB connection is not enough to program the MSP430G2553, you need to wire a MSP430 FET tool (MSP-FET, eZ-FET, eZ430, etc.) to the Spy-Bi-Wire (J3) connector of the DRV8702-Q1EVM in order to program the device. Please see the MSP Debuggers…
Part Number: DRV8702D-Q1EVM Other Parts Discussed in Thread: CSD18540Q5B , DRV8702-Q1EVM The kit worked great once I found that the Sleep Button state was backward. I assumed Enabled was to drive the signal low. After using a DMM I found that the state…