Part Number: DRV8718S-Q1EVM Other Parts Discussed in Thread: DRV8718-Q1 , Hello sir ,
1)I am using DRV8718-Q1 EVM board , am also changing the PWM value of input but there is no output coming . Please tell me how can i use this EVM board .
2) There are…
Part Number: DRV8718S-Q1EVM I am trying to control ORVM( Outer rear-view mirrors) Re by establishing communication between an Arduino and DRV8718S-Q1 using SPI communication protocol
but motor is not rotating , sometimes output1 and output2 gets same voltage…
Part Number: DRV8718S-Q1EVM Other Parts Discussed in Thread: DRV8718-Q1 , DRV8714S-Q1EVM Hi Motor Drive Team,
I have a customer interested in example source code for the DRV8718-Q1. We found this previous e2e post that mentions source code for the EVM,…
Part Number: DRV8718S-Q1EVM Hello,
we have design which has 3 motor running and are connected to DRV8718S.
for running 3 motor, we made H-bridge circuit with FET.
if it is in no battery status, if first motor makes induce voltage, could that voltage…
Part Number: DRV8718S-Q1EVM Other Parts Discussed in Thread: MSP-FET , UNIFLASH Hi Team,
Could you please kindly help to check if below firmware could be used to in DRV8718S-Q1 EVM(the EVM is sampled two weeks ago)? Or if customer need to do firmware update…
Part Number: DRV8718S-Q1EVM Hi Team,
Could you please kindly help to check for input bulk capacitor, if we have some formula which could recommend for customer to do their design? Form datasheet, we can only find some points which would impact the selection…
Part Number: DRV8718S-Q1EVM Other Parts Discussed in Thread: DRV8718-Q1
When I use the DRV8718S-Q1 EVM, i set the EVM in PWM mode to control the low side MOSFET, I found that there will be a step when the GL1 pin is high (as shown in the picture above…
Part Number: DRV8718S-Q1EVM The chip select (nSCS) of the DRV8718 EVM takes way more current to pull it low than what's in the datasheet.
Datasheet: 50 uA (100 uA max)
Reality: 45 mA!
I'm using the 14 pin MCU to DRV header of the EVM and just…
Part Number: DRV8718S-Q1EVM Hello Everyone,
I would like to know the Part Number of components used for reverse polarity protection of DRV8718S-Q1EVM.
Does any one have the corresponding BOM ?
Looking forward for the quick response,
Thanks and Regards…
Part Number: DRV8718S-Q1EVM
Hello Team,
My customer is having issue in the SPI bus on the 14 pin MCU to DRV header of the EVM it is not functioning. Driving the SDI pin with a microcontroller yields wilding undefined behavior. I think I found the issue…