Part Number: DRV8801A-Q1 Other Parts Discussed in Thread: DRV8801 Hi, if we power the DRV8801 from 24V, would the output be able to drive +-/12V?
Thanks,
Jeramie
Part Number: DRV8801A-Q1 Other Parts Discussed in Thread: DRV8873 , DRV8143-Q1 , DRV8873-Q1 Hi team!
The customer wanted to use DRV8801A-Q1 to provide single direction current, such as using PWM control OUTA upper switch, and OUTB lower switch is always turn…
Part Number: DRV8801A-Q1 Hey Team,
In old Datasheet (SLVSC79C), the Charge pump voltage is mentioned as Vbb+7 whereas in new Datasheet (SLVSC79D) it's mentioned as Vbb+17.
Is this a change or typo?
Old:
New:
Best, Dajon McGill
Hi Gregor,
The datasheet specification when the voltage on the VBB pin is increasing (ramping up) the UVLO threshold could be a maximum of 7.5 V. The DRV8801 was designed and guaranteed to operate from 8 V to 38 V. When an UV is detected the outputs of…
Part Number: DRV8801A-Q1 Hi Team,
With the DRV8801A-Q1 in automotive applications is there any protection devices we recommend when using off battery?
Big electrolytic? TVS?
Thanks,
David
Part Number: DRV8801A-Q1 Hi
Ti Team,
I need a Ibis model for above part number DRV8801A-Q1 for my SI / PI Simulation
please provide me for my personal mail.
let me any further details is required.
Thanks & Regards
Sathya KR
Other Parts Discussed in Thread: DRV8801A-Q1 Hi~
During the production, customer want to test motor without board power supplied.
It means, after SMD, they just want to test motor by supplying +12V at OUTA/OUTB without supplying power at VBB.
Absolute…
Part Number: DRV8801A-Q1 Hello Team,
Kindly help me with the calculations required to find the value of Inductor which should be kept in series with the MOTOR winding between the H-Bridge outputs. This Inductor is used to limit the inrush current along…
Part Number: DRV8801A-Q1 Other Parts Discussed in Thread: DRV8703-Q1 , DRV8801 , Can i drive an external FET for reverse battery protection using the charge pump of the DRV8801A-Q1? There is no information in the datasheet about the charge pump. In the DRV8703…
Part Number: DRV8801A-Q1 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Hello All,
Could you please share some link or some suggestion to do simulation on this driver in Pspice or Simetrix.