Hi Danilo,
I don't see any issues with the schematic that could explain the damage to the IC. However, I did notice the exposed thermal pad in the layout is small compared to the DRV8876EVM. During heavy loads, the current will spike up and the heat…
Hi Rick,
I think the issue here is that you are providing a very high PWM frequency. The DRV8876 has accept a maximum PWM frequency of 100kHz. With your current set-up, the frequency is 714286kHz which is very high for this device. Can you try to decrease…
Other Parts Discussed in Thread: DRV8876 , DRV8837 , DRV8837C , DRV8874 We drive all kinds of motors including Brushed, Brushless, and Stepper varieties.
What about Servo Motors?
Yes we are can include those as well. A servo like the one below has…