Part Number: DRV8912-Q1EVM Hello,
I bought DRV8912-Q1EVM for testing DC motor actuator and tried to run it with control SW, SLVC759-DRV8912-Q1EVM GUI (Version: 1.1.2) and DRV8912-Q1EVM-WEB-GUI – Web-based GUI for DRV8912-Q1EVM (Version: 1.0.7) which…
Part Number: DRV8912-Q1EVM Other Parts Discussed in Thread: DRV8912-Q1 Hi, Support Team
We use DRV8912EVM to control Motor driver; We find EVM can not workable also measurement output #1 and output# 2 are no signal.
Measurement point and signal chart: …
Part Number: DRV8912-Q1EVM Hi TI team,
We use DRV8912-Q1EVM to connect the three-way valve for load test. One end of the three-way valve is connected to OUT4/6/7/9 and the other end is connected to OUT3/10/11/12. During the process of controlling the…
Part Number: DRV8912-Q1EVM Other Parts Discussed in Thread: DRV8908-Q1 , DRV8912-Q1 Hello
Please provide the CE/EU Declaration of Conformity for this SKU (the CE/EU Declaration of Conformity must cover both the board as well as the USB cables that is included…
Part Number: DRV8912-Q1EVM The documentation for the DRV8912 EVM board says it has a 3A total current limit, while the IC is rated to 6A. What is the driving this limitation? Thermal management or another component?
I am making a prototype that needs…
Hey Jass,
I found one DRV8912EVM in the lab to try to test this with, but the EVM is damaged and unusable. I have ordered new EVMs that will take a week to get here. There is another EVM in the lab I can try out later this week, please give me a few days…
Part Number: DRV8912-Q1EVM Other Parts Discussed in Thread: DRV8912-Q1 hi, i have two arduino, arduno due 3.3V and DRV8912-Q1EVM works good the soleonid, but with arduino atmega2560 (5V) i cant do work the solenoid, i have osciloscopy and i cant see any…
Part Number: DRV8912-Q1EVM Other Parts Discussed in Thread: DRV8912-Q1 Is there a way to controlling the chip with code and to be able to go back and forth between the GUI easily?
Hey Cherry,
Per 8.3.1.1.1 Continuous Mode (Without PWM) , The half-bridges are configured to operate in the continuous mode without using any PWM switching by default. Any high-side or low-side switch is switched on by individually setting the high-side…