Part Number: DRV8955 Other Parts Discussed in Thread: DRV8935 , Tool/software: Please help and check below issue:
1. Model: DRV8935/DRV8955
2. When IN1 is in logical "1" state, what's the OUT1 state? High or Low?
There is an issue I think it need…
Part Number: DRV8955 Other Parts Discussed in Thread: DRV8952 , DRV8962 Tool/software: Dear TI Support Team,
I have made a DRV8955/DRV8923 test board and tried several methods to get the motor running.
The schematic had also been previously provided…
Part Number: DRV8955 Other Parts Discussed in Thread: DRV8844 , DRV8962 Hi BU,
My customer is currently looking at DRV8955 but its Vs is only fixed to 48V. It is not suitable for his project as the Vs is +56V.
Do we have any other suitable BDC which…
Part Number: DRV8955
Tool/software:
Hi All,
I'm looking to use the DRV8955 to drive a solenoid valve open and closed as quickly as possible. I would also like to utilize the ITRIP feature to limit the current from exceeding a threshold, as well…
Part Number: DRV8955 Other Parts Discussed in Thread: SN754410 , LM339 , NE555 , LM393 , DRV8962 Tool/software:
I believe I found an excellent choice for upgrading my motor driver however, no reference design exists and I couldn’t find one schematic…
Part Number: DRV8955 Dear All,
we are using the DRV8955 motor driver. We set its MODE to 330kOhm to GND (four independent High-Z, voltage on MODE_1.23V) and IN1-4 and EN1-4 pull to GND.
After that if we pull-up any one output by 1kOhm to VM=12V and…
Part Number: DRV8955 Tool/software: hi team,
my customer wants to use DRV8955 to connect the capacitive load in digital output module.
Will it cause any problems? thanks!
Part Number: DRV8955 Tool/software: Hello,
The following post is related to this one: https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1438789/msp430f2617-pwm-output-with-4ms…
Part Number: DRV8955 Other Parts Discussed in Thread: DRV8962 , Tool/software: Can you describe the spread spectrum behavior of the DRV89xx series? I am looking at controlling a proportional valve for a pressure controller, but I think the spread spectrum…