Part Number: DS250DF810 Other Parts Discussed in Thread: TUSB1104 , SN65DP141 , TDP142 , TDP2004 , TUSB2044 Dear team,
Do we have suitable solution can replace below? Thanks a lot.
Item
Signal
RVP using model
Description
Vendor
1
USB3.2…
Part Number: DS280DF810 Other Parts Discussed in Thread: DS250DF810 , Hi Team,
I check below link but I would like to double check that if DS280DF810 can P2P replace DS250DF810 at hardware part, and at software part no need to change software code at <…
Part Number: DS250DF810 Other Parts Discussed in Thread: DP83869
HI there,
I hope you are well,
I have some questions regarding the correct way to connect this device inline with 2 ethernet connectors (RJ45), as if this device was in the middle of…
Part Number: DS250DF810 Hi, We have used DS250DF810 in 40G backplane application, here are 4 DS250DF810 on one board, ADDR are set to 0x30.0x32.0x34.0x36.
And we tied all DS250DF810's EN_SMB(E3) to 2V5, READ_EN_N(F13) is floating, ALL_DONE_N is floating…
Part Number: DS250DF810 Hi Team,
Could you please share the IBIS_AMI model for me? I find there is a request link in the E2E, so I also request on that. Please let me know if that method is correct. Thanks.
https://www.ti.com/licreg/docs/swlicexportcontrol…
Part Number: DS250DF810 Other Parts Discussed in Thread: DS280DF810 TI technical personnel,
Regarding the DS250DF810 and the DS 280 DF810:
What are the explicit differences?
Are they pin compatible?
Is the upper limit of the 28Gbps operation offered by…
Part Number: DS250DF810 Hello,
Any chance that device characterization data exists for 10.3125Gbps data rate ? I'm interested in following parameters :
JTJ Output Total jitter (TJ)
JRJ Output Random Jitter (RJ)
Especially for JTJ: Will it stay…
Part Number: DS250DF810 Other Parts Discussed in Thread: DS110DF410 Hi,Engineer
Can I ask you a question? We have a project use DS250DF810 Retimer connection ASIC to 10G SFP+ Optical,
ASIC support SFI and KR protocol,KR protocol can route a long traces…