Part Number: DS250DF810EVM Hi gent.,
May I know if the DF810EVM has soldered 1x8 MXP connector? Also, which cable is recommended here if we run it at 25Gbps. thanks.
Steven
Part Number: DS250DF810EVM Other Parts Discussed in Thread: SIGCONARCHITECT
Would like to use this DS250DF810EVM with SigconArchitect GUI with wRTE V2.0.0.8 but come with LabVIEW issue.
Which version of LabVIEW I shall install? Can use community version…
Hi Rodrigo
OK greats. By the way, EVM can act as receiver and validate the result? And 16 EVM (transmit & receive), any alternative to control those 16 EVM by single console? Any application to overcome this request?
Best regards,
Thomas
Other Parts Discussed in Thread: DS250DF810EVM Would like to know below setting is workable or not
DS250DF810EVM (Tx) > DUT > DS250DF810EVM (Rx)
Without using any signal generator
To measure eye diagram.
Hi,
The DS250DF810 cross-point block is located before the CDR, so its configuration is not affected by it. However by default the retimer channel output is muted when CDR is not locked.
Cordially,
Rodrigo Natal
HSSC Applications Engineer
Part Number: DS250DF810EVM Other Parts Discussed in Thread: DS250DF810 , , LMH1218 I am using SigCon on the DS250DF810EVM. It comes up connected on 0x30 but it reads that the device is a LMH1218 and not DS250DF810. I added a device as per the guide but it…
Part Number: DS250DF810EVM Other Parts Discussed in Thread: DS250DF810 I cannot get the DS250DF810 to fanout when the CDR is not locked. I need to use this part some of the time when the CDR is not locked for one bit rate we are using. I know you have…
Part Number: DS250DF810 Hi Team,
What’s DS250DF810EVM interface? I will integrate it into my LabView code, are LabView/python drivers available?
Thanks,
Shlomi
Part Number: DS250DF810EVM Other Parts Discussed in Thread: DS250DF810 Can I use the above EVM to drive LVDS Pulse signal with the following criteria:
VCM: 0.4V – 1V
VDiff: 150mV – 800mV
Pulse width: 0.7ns – 3ns
Trise/Tfall: 20ps – 5…