Part Number: DS90LV011A Kindly help with more details related to DS90LV011A.
Maximum loads can be connected to (Multidrop)
Maximum distance supported
Maximum Speed which can be supported with Max Load , Max Distance.
Have looped in customer for direct…
Part Number: DS90LV011A Hello team,
I'd like to know if the DS90LV011A TTL input can accept partial power down sequence. In other words, is there any problem on the use case of Vin=3.3V with Vdd=0V?
Thanks in advance. S.Sawamoto
Part Number: DS90LV011A Maybe I overlooked it, but can someone tell me what the current planned end-of-life is for the DS90LV011A component?
What are current lead times for order and shipment for this component as well?
Part Number: DSLVDS1001 Other Parts Discussed in Thread: DS90LV011A , Hi Team
I am confusing on how to select between DSLVDS1001 and DS90LV011A ,they are almost same in datasheet description,care the performance,cost is not important
Hello Muthukumar,
Just for clarification, are you requiring a device that can support 100 MHz ( 200Mbps ) signal or 48 Mbps?
We have LVDS devices capable in reaching those data rates. Please look at LVDS driver ( DS90LV011A ) and LVDS receiver ( DS90LV012…
Part Number: DS90LV011A Other Parts Discussed in Thread: SN74AUC2G53 , SN74LVC1G3157 Hi Team,
I looking for low jitter buffer to 2 different clock as attached.
I generate 2 clocks: one from external source and second internal and than I need to choose…
Part Number: DS90LV011A Hello support team,
I want to know the thermal resistance "θjc" of DS90LV011A. Could you teach me it?
Best regards, M. Tachibana
Part Number: DS90LV011A I'm driving the DS90LV011A with an oscillator chip. Does there need to be any termination at the input of the DS90LV011A? How about series resistance at the output of the oscillator chip? Figure 4 shows a 50 ohm shunt termination…
Part Number: DS90LV011A Hi Team
My customer would like to use DS90LV011A to drive RJ45 from FPGA LVDS signal, the application is one board FPGA to another board FPGA communication (very similar to PHY), data rate is about 100MHz.
If DS90LV011A not ok…