Part Number: DS90UB936-Q1 Hi Team,
We have one suspected system that crystal can't output 26MHz to 936. We want to check if there is any spec for 936 driving level.
The crystal spec driving level requirement is 0.01uW.
Regards,
Roy
Part Number: DS90UB935-Q1 Other Parts Discussed in Thread: DS90UB936-Q1 , CAM module( DS90UB935-Q1 ) --> DS90UB936-Q1 --> SoC(MIPI_CSI) and NPU(BT656)
Can the above architecture be implemented?
1. One SerDes output to DS90UB936-Q1.
2. DS90UB936-Q1 output…
Part Number: DS90UB936-Q1
Hi Team,
I have few questions would like to check with you.
1. According to the content, "Each RX port signal path continuously monitors cable characteristics for long-term cable aging and temperature changes." Does…
Part Number: DS90UB936-Q1 As I understand from the Pin description table, we need to pull VDD_SEL = LOW to have the 1V1 rail be internally generated.
However, the connection of VDD_SEL to 1.8V in Figure 8-4 of the datasheet, appears to contradict this…
Part Number: DS90UB936-Q1 Other Parts Discussed in Thread: DS90UB953-Q1 , DS90UB936-Q1 pair with DS90UB953-Q1
1. can DS90UB936-Q1 support 1080P@60Hz or @30Hz
2. can I input 1080p@60 or @30Hz to both FPD-Link
3. how calculate the max. resolution of device …
Part Number: DS90UB936-Q1 DS90UB935-Q1
Hello Expert,
I am new to this serializer functional safety test. What is the right approach to perform the safety test and what need to be cross checked / monitored during this test. Please guide here.
do we need…
Part Number: DS90UB936-Q1 Hi expert,
Customer do the ESD test to DS90UB936-Q1.
Background:
1) When ESD test is carried out on 936, interrupt would happen and GPIO3/INTB would be low.
2)SOC would receive the interrupt and clear interrupt on 934, then GPIO3…
Hi Yuan,
I'm looking into this while Zoe is OOO through early next week.
Da Yuan said: 1> Below steps is our current improved solution. We tried more than 300 times SOC resets in vehicle, the problem did not recur. Can we use this solution, or soft…
Part Number: DS90UB936-Q1 Hi Team,
My customer would like to test STP connection from a 953 EVM to a 936 EVM, it is my understanding that we don't have any default EVMs that can do this so I have tried to document all the changed that will be needed below…
Part Number: DS90UB936-Q1 Hi team,
My customer meet EMC issue and they want to use half rate mode in sync mode.
Do they only need to change the 0x58? We didn't see many description in the datasheet.
And could you please help check if it will be good…