Part Number: DS90UB960-Q1 Other Parts Discussed in Thread: DS90UB9722-Q1 , DS90UB941AS-Q1 , DS90UB983-Q1 DS90UB960-Q1,DS90UB9722-Q1,DS90UB983-Q1,DS90UB941AS-Q1 this all mentioned parts are Grade 2: –40℃ to +105℃.Is there are Grade 1:–40℃ to +125℃ part numbers…
Part Number: DS90UB941AS-Q1 Hi team,
The DS90UB941AS-Q1 has a VDDIO supply of 1.8V. However, the IIC pull-up is 3.3V. Is this acceptable?
Thanks
Xiaoxiang
Part Number: DS90UB941AS-Q1
Hello TI team,
The 941 Datasheet mentions that the maximum PDB PIN is 100uA, but the GPIO configurable range of MCU is 2mA~16mA. Q1: it looks like 2mA > 100uA. Will this damage PDB PIN? I think a lot of MCU's GPIO output…
Part Number: DS90UB941AS-Q1 Tier1 Tianma/ OEM VW
Hi Team,
config: SOC-941-948-slave
My customer wan t to access the 948 register from SOC, I would like to know what register i need to configure to enable the I2C pass through for this operation:
Should…
Part Number: DS90UB941AS-Q1 Dear expert,
Customer config BRIDGE_CFG2 Register (Address = 0x56) as DSI Reference Clock Mode.
When they stop DSI traffic including DSI clock, does UB941 switch to internal reference clock to LOCK FPDlink automatically?
I know…
Part Number: DS90UB941AS-Q1 Hello Team,
I got question from my customer if 941AS support interrupt in case error case.
I understand this is for passing INTB_IN at DES to INTB at SER. but I also found bit6 that indicate LOCK for INTB.
I think this is…
Part Number: DS90UB941AS-Q1 Other Parts Discussed in Thread: ALP , USB2ANY Hello TI team,
Why did 941 register reset itself?
We encounter occasional flickering/black screen phenomenon, and the software detects that the 924_LOCK is link down;
Verify…
Part Number: DS90UB941AS-Q1 Dear Team,
I am using DS90UB941AS in my design.
I know this will convert DSI to FPD.
I need to convert this FPD to RGB.
Can you suggest any IC for the same(FPD to RGB)
Regards
HARI
Part Number: DS90UB941AS-Q1 Hi experts,
we have a issue for i2c communication NAK on local bus, after reproduce this issue, we found that remote i2c bus stuck low for long time. please help us to find the root cause.
MCU( 0x6B ) is setup as ( 0x6D…