Part Number: DS90UB960-Q1 Other Parts Discussed in Thread: DS90UB9722-Q1 , DS90UB941AS-Q1 , DS90UB983-Q1 DS90UB960-Q1,DS90UB9722-Q1,DS90UB983-Q1,DS90UB941AS-Q1 this all mentioned parts are Grade 2: –40℃ to +105℃.Is there are Grade 1:–40℃ to +125℃ part numbers…
Part Number: 5-6KINTERFACE
Dear TI
At present, the measured data of EMC current exceeds the standard. The detailed test steps are shown in the attachment. The interference sources obtained in the experiment are 1.7M apart. The interference sources…
Part Number: DS90UB960-Q1 Hi,
I would like to implement the next setup-
I set the 960 that CH0 to CSI0 and CH1 to CSI1 but it didn't work.
When I set a test pattern at 953 and sending the CH0 and CH1 to CSI1 it's working.
What I'm missing.…
Part Number: DS90UB960-Q1 Hi team,
Did the DS90UB960-Q1 has a LOCK PIN?
If customer want to use the MCU GPIO to detect the lock of DS90UB960-Q1, which PIN of ds90ub960-q1 can be used?
Thanks
Xiaoxiang
Part Number: DS90UB960-Q1 Other Parts Discussed in Thread: DS90UB953-Q1 , , Good afternoon,
We're trialing a few PCB stack-ups for the best signal integrity to 4 x DS90UB953-Q1 devices (using RG-178 coaxial cable at 3 metre lengths) and appear to be…
Part Number: DS90UB960-Q1 Hi,
I used the Code Example for Pattern Generator.
It works to CSI0.
When I tried to use the same code to CSI1 it didn't work and I didn't see anything.
What might be the problem?
BR
Shmuel
Part Number: DS90UB960-Q1 Hi expert,
I saw many script config 0x6D PORT_CONFIG to 0x7C while bit 2 is a reserved register.
Do we have to write 1 to bit 2 for normal operation?
Thanks!
Now pattern generation is working I can see the straming data on raspberry pi. lane conifguration was not correct in pattern gen code
v4l2-ctl --stream-mmap --stream-count=-1 -d /dev/video0 --stream-to=/dev/null
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<…
Part Number: DS90UB960-Q1 Hi, Support team.
I'm currently working on ADAS project and investigating the architecture. As we are targeting on the ASIL D redundency idea, thus we would like to understand if there is possibility of have some new topology…
Part Number: DS90UB960-Q1 Hello Experts,
at the moment I am facing some difficulties. We have a camera from a customer using the serializer DS90UB933. This camera should be visualized with our device using the DS90UB960. Colorformat YUV 8 bit.
I've already…