Part Number: DS90UB962-Q1 Other Parts Discussed in Thread: DS90UB935-Q1 , DS90UB953-Q1 The changes in the camera aspect of the new project compared to the old project are as follows:
1. The resolution has changed from 1920 * 720 to 1920 * 1440
2. The serializer…
Part Number: DS90UB962-Q1 1,Can the setting of the 962 mode pin be modified again through I2C after power on.
2: What is the maximum bandwidth supported by 962 LANE for 3G?
3: The current MODE setting is RAW10, with a camera of 1920 * 1440, 30fps, and…
Part Number: DS90UB962-Q1 Other Parts Discussed in Thread: DS90UB953-Q1 Hi team,
As shown in the attachment, the 962 register detects the existence of CSI ERROR in the video data: 1. Is CSI ERROR a problem with the link between the 962 deserializer and…
Part Number: DS90UB962-Q1
I would like to ask why our camera can receive signals of up to 4x3Gbps when our intelligent output has a maximum bandwidth of 4x1.6Gbps?
Part Number: DS90UB962-Q1 Is there a testing method that can reproduce ECC Error? For example, constantly switching video streams? Or ECC errors caused by hardware LINK disconnection/connection?
Because the customer hopes to have a reproducible ECC error…
Part Number: DS90UB962-Q1 Hi,
Could you please tell me what the following statement in Revision History means? • RESERVED register bits 0x20[3:0] that have no customer use case................................... ......................69 • RESERVED…
Part Number: DS90UB962-Q1 Other Parts Discussed in Thread: DS90UB933-Q1 Hi team,
My customer is PATEO and the OEM is Dongfeng. When they only used DS90UB962, they encountered the problem that the surround view camera did not transmit images.
The connection…