Part Number: DS90UH928Q-Q1 Hello team
We'd like to make sure about configuration to achieve customer required operation.
They'd like to transmit LVDS CLK during Lock=low. Is suppose that we can achieve this condition by
0x02 bit6(OEN/OSS_SEL)…
Part Number: DS90UH928Q-Q1 Other Parts Discussed in Thread: DS90UB928Q Dear Sir/Madam,
Can i know if i will need to be a HDCP adaptor license user in order to buy the part:
DS90UH928QSQX/NOPB?
Best regards, KPK
Part Number: DS90UH928Q-Q1 Hello Expert,
I'd like to confirm about CMLOUT behavior. Will CMLOUT stop transmission during 928 loss a Lock? If CMLOUT continue to transmit the signal, what signal will be transmitted?
Best regards, Kazuki Kuramochi
Part Number: DS90UH928Q-Q1 Hi expert,
My customer is tring HDCP between DS90UH928Q-Q1 and DS90UH925-Q1.
However, HDCP cannot be enabled. they cannot understand the reason.
They are tring several setting for SER/DES devices.
Could you please give me your…
Part Number: DS90UH928Q-Q1 Other Parts Discussed in Thread: DS90UH927Q-Q1 ,
Hi Expert,
My customer have an issue about HDCP blue display during short period (around 0.2sec)
It seems to be retry automaticaly betwee SER and DES devices.
Also, It was occered…
Part Number: DS90UH928Q-Q1 Hello team,
Could you let me know if the combination between DS90U B 925-Q1 and DS90U H 928-Q1 can establish the link?
If we need register setting to achieve this could you let me know how to set?.
Thanks.
Regards,
Hirata
Part Number: DS90UH928Q-Q1 Hello FPD-LINK teams,
Do you mind helping to have a look on below issue of DS90UH928Q-Q1?
LVDS‘s CLK signal has 2 stages but there is only one power supply, 3.3V
CH3 is CLK signal of LVDS. What other signals can effect…
Part Number: DS90UH928Q-Q1 Hello, Team,
Could you please tell us the difference between X, Static, and Active on the Table 5?:
*datasheet p31, Table 5
What does X, Static, and Active of "SERIAL INPUT" each mean in this context?
Best Regards…
Part Number: DS90UH928Q-Q1 Dear Sirs,
Customer use UH941 paired with UH928 is failed, the display is wrong.
But UH941 paired with UH948 is OK.
The schematics as attached.
AP02-Main-V1 (1).pdf
iMX8-SerDes-V1 (2).pdf
Please help to review if there is anything…
Part Number: DS90UH928Q-Q1 Hi Team,
When the 928 is used in single channel mode but paired with an HSD+2 connector where two of the four data cables are not used, how should those unused cables be terminated? Should they be grounded or AC coupled to ground…