Part Number: DS92LV2411 Hi Team,
I couldn't find the package details for the RHS 48 pin in our DS,
can you advise where can i find this information?
Best regards.
Part Number: DS92LV2411 Hi team,
The device rated LVCMOS I/O voltage between 0.3V - VDD +0.3V, for voltage overshoot/undershoot cases, is there a maximum diode current to refer to?
Regards
Part Number: DS92LV2411 Other Parts Discussed in Thread: DS92LV2412 , Hi,
DS92LV2411 and DS92LV2412 are used to communicate between the main board and the sub board.
Currently, communication is possible when the distance between the boards is about 500…
Part Number: DS92LV2411 Other Parts Discussed in Thread: DS92LV2412
Hi Team,
I want to consult the pin function of DS92LV2411. There is a pin function table on page 3 of the data table for DS92LV2411. There is an item of "type" on the table, which says…
Part Number: AM3352 Other Parts Discussed in Thread: DS92LV2412 , DS92LV2411 ,
Hi,
The AM3352 and LCD are not directly connected, but are configured as AM3352 → LCD serialiser(DS92LV2411) → LCD deserialiser(DS92LV2412) → LCD. The flickering frequency increases…
Part Number: DS92LV2411 Other Parts Discussed in Thread: DS92LV2422 , DS92LV2421 , DS25BR100 , DS92LV2412 , I need to design a 24 parallel lines SerDes Transceiver whose serial lines can run about 70 feet. Any IC recommendations or design ideas?
Hello Daniele,
you can use the following SER with the DS92LX1622 deserializer. However, all of these devices are older than the DS92LX1621.
DS92LX2121, DS92LV2411, DS92LV2421 ...etc
Same thing, there are other Deserializers, but these are older than the DS92LX1622…
Part Number: DS92LV2411 Team,
For 24-bit TFT LCD Display that uses the TI DS92LV2411 and DS92LV2411 serializer/deserializer combo for transmitting display signals via LVDS. Are these ICs still the way to go for new designs? Is there anything better to use…
Part Number: DS92LV2411 Other Parts Discussed in Thread: DS92LV2412 , Hi Team,
Our customer is observing UNLOCK on DS92LV2412 Deserializer.
Do you have PCLK input jitter requirement on Serializer DS92LV2411 side or any recommendation ?
Best Regards,
Ka…
Part Number: DS92LV2411 Other Parts Discussed in Thread: DS92LV2412 Hello,
I want to know coplanarity and standoff parameter of the below devices:
DS92LV2411
DS92LV2412
But I can’t find these information in the datasheets.
I think QFN/SON package…