Part Number: DSLVDS1047 Other Parts Discussed in Thread: ADS7038 , DSLVDS1048 Hi Team,
our customer wants to use the DSLVDS1047 / DSLVDS1048 in a very time critical control loop with our ADS7038.
In order to be 100% sure that we do not have timing issues…
Part Number: DSLVDS1047-1048EVM I would like to get the physical dimension for the board as well as the cutout pattern need for mounting.
Could anyone please provide me with those?
Part Number: DSLVDS1047 Hi Expert,
Does DSLVDS1047 have internal clamp diode between DIN and Vcc?
I believe this device have diode, because the Abs max of DIN is Vcc+0.3V.
Customer is considering abnormal condition about applying any signal to DIN during…
Part Number: DSLVDS1047 Hi Expert,
My customer have a question,
If they use 60ohm termination resistor, how the device work? They think that the amplitude of the output voltage will be smaller. Is it correct?
Of course, they understand LVDS should be…
Part Number: DSLVDS1047 The current raised 438mA when we input 20MHz square wave in DSLVDS1047-1048EVM . And now we connected 1047 to 1048 using one twist cable which is 80cm lenth . So anyone can help to explain why the current is so high .
Thanks!
Part Number: DSLVDS1047 Can signal be transmitted in more than 100-meter cable using DSLVDS1047. (clock frequency is less than 10MHz)? if not which chip can do?
Part Number: DSLVDS1047 Dear All
In Spec of DSLVDS1047 , some information as below mabe not be appeared . Figure 25 just be a graph of consumption vs frequency.
Figure 25 shows very good typical performance that can be used as a design guideline for data…